IMX6Q EIM (16bit :D0~D15) problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Q EIM (16bit :D0~D15) problem

997件の閲覧回数
jianminli
Contributor I

We're using i.MX6Q with EIM interfacing to an FPGA, using synch 16 bit none multiplexed mode with burst mode.

we use EIM_D0~EIM_D15 as DATA bus;

address and data bus work well except EIM_D6 and EIM_D7:   when it pull down , it is hard to be pull up.

so if i want it to give a 101 level ,but it actually give me a level of 100.

why?    is there some hardware problem?

ラベル(1)
タグ(1)
0 件の賞賛
5 返答(返信)

752件の閲覧回数
329982628
Contributor I

您好

想问一下楼主解决这个问题了吗

最近开发遇到了相似的问题~

邮箱号 329982628@qq.com

望回复 谢谢

0 件の賞賛

752件の閲覧回数
jianminli
Contributor I

The configuration of the pin is incorrect.

0 件の賞賛

752件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jianmin

yes this may be hardware problem, please try to set these pads as

gpios and toggle them. May be useful to test board with jtag and baremetal test SDK:

Github SDK
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

752件の閲覧回数
jianminli
Contributor I

I have set these pads as gpios and toggle them,the first picture is the performence of EIM_D6 or EIM_D7,

The second picture is the performence of other EIM DATA pins .

I checked the hardware connetion,and  there is nothing wrong.

is there any possible that the chip(mx6q) itself has something bug with EIM_D6 and EIM_D7? I tried some other imx6q chips,and got the same result. Can u help me ?

 abnomal.jpg

normal:

normal.jpg

0 件の賞賛

752件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

had you tried baremetal sdk example. Please try it, set eim with low frequency,

for example with 20MHz.

Best regards
igor

0 件の賞賛