MCIMX8M-EVKB: need help getting started with Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX8M-EVKB: need help getting started with Linux

Jump to solution
4,382 Views
mditto1
Contributor III

I'm trying to use the MCIMX8M-EVKB for the first time and I can't get it to boot Linux from an SD card.

The Quick Start Guide says to check www.nxp.com/imx8mquadevkB for software and info, but that URL gets a Page Not Found error.  Removing the trailing B leads to the main MCIMX8M-EVK page, where I find a link to Get Started with the MCIMX8M-EVK.  This contains a Linux chapter which explains using a .sdcard file to create a bootable SD card, and suggests using the Linux download page, which is nothing but a .tar.gz file.  This archive contains only one file with "sdcard" in its name - fsl-image-qt5-validation-imx-xwayland-imx8mqevk.sdcard.bz2.  I assumed that I should pipe this through bunzip2 and onto an SD card, which I did, and this resulted in the SD card with valid-looking boot and root partitions, which I can read on my Linux development machine.  But nothing happens when I boot the EVK with this SD card inserted.

I have the serial cable working - I can boot and interact with the Android image on the eMMC.  But when I change SW801 to 1100 and power on (with the SD card inserted) there is no activity on the serial port nor the HDMI output.  The red power LED lights but that's the only sign of life.

How do I get a Linux image on an SD card and boot it?  I would prefer to use the serial console and not use a monitor.

Thanks,
Mike

0 Kudos
Reply
1 Solution
4,198 Views
mditto1
Contributor III

I found an sdcard image in the L5.4.70_2.3.0_MX8MND3L BSP download, and it just works, no trouble at all.  I downloaded it from here:
https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

The command to write it to an SD card:
dd if=imx-image-full-imx8mqevk.wic of=/dev/sda bs=1048576

I don't know what is wrong with the sdcard image in the "Get Started" and "Linux download" pages, but the one in the BSP package (".wic" file instead of ".sdcard") works fine for me and my problem is solved.

Cheers,
Mike

View solution in original post

0 Kudos
Reply
9 Replies
4,199 Views
mditto1
Contributor III

I found an sdcard image in the L5.4.70_2.3.0_MX8MND3L BSP download, and it just works, no trouble at all.  I downloaded it from here:
https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

The command to write it to an SD card:
dd if=imx-image-full-imx8mqevk.wic of=/dev/sda bs=1048576

I don't know what is wrong with the sdcard image in the "Get Started" and "Linux download" pages, but the one in the BSP package (".wic" file instead of ".sdcard") works fine for me and my problem is solved.

Cheers,
Mike

0 Kudos
Reply
4,349 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi mditto1,

 

The quick start guide is a good way to start but it has some missing points, please review the Linux guide that comes with the BSP, chapter 4.3 preparing an SD/MMC card to boot.

https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf

 

Regards,

Israel H.

0 Kudos
Reply
4,345 Views
mditto1
Contributor III

I had seen that document and tried to find some clues there, but I don't see why those steps wouldn't have already been done to the prepared .sdcard image on the NXP download page.  My best guess is that the wrong version/build of U-Boot has been included in the .sdcard image, so I did try the command in 4.3.4 with what seemed like the right U-Boot image, but it didn't help.  The image I copied was imx-boot-imx8mqddr4arm2-sd.bin-flash_ddr4_arm2 , should that have worked?  Is there anything else needed to get the board to load U-Boot from the SD card, perhaps a boot sector or something?

 

0 Kudos
Reply
4,334 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi mditto1,

 

Could you review the ROM configures the boot media and attempts to read the image from a predefined address in the boot device, probably the boot media is trying to start from a different address, all of this comes on the reference manual but see the table below:

Selection_429.png

 

Also please take a look into the next post, hope this help you:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-Boot-process-and-creating-a-bootab...

 

Regards,

Israel H.

0 Kudos
Reply
4,314 Views
mditto1
Contributor III

Hi, Israel, thanks for the information.

i.MX Linux® User's Guide section 4.3.4 says boot offset is 33 k for i.MX 8M Quad.
i.MX8 Boot process and creating a bootable image table 5-22 says boot offset is 32 k.
The .sdcard image on the download page has a bootloader image at 33 k.

I've tried both locations, still no signs of life.  Can you confirm I am using the right U-Boot image?
imx-boot-imx8mqddr4arm2-sd.bin-flash_ddr4_arm2

i.MX8 Boot process and creating a bootable image table 5-8 says boot switches should be 0011, I'm assuming that means ON-ON-OFF-OFF as described elsewhere.

Mike

0 Kudos
Reply
4,291 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi Mike,

 

No, that U-boot file is one we usually use to validate our DDR4 boards, please use the imx-boot-imx8mqevk-sd.bin-flash_evk, a tell me if this works for you, follow the same as Linux user's guide 4.3.4 to flash the SD card.

 

Also, you can use Yocto to create and compile the image for your device, just to discard problems that may come with your image. Please follow the documentation that comes with the BSP.

 

Hope this helps you.

Regards,

Israel H.

4,281 Views
mditto1
Contributor III

No, no difference.

I wonder if it's because I'm using an SDHC card.  Maybe the boot ROM doesn't support SDHC but U-Boot does (thus it works when I load U-Boot from eMMC)?

 

0 Kudos
Reply
4,295 Views
Luishernandez1
Contributor II

.

0 Kudos
Reply
4,371 Views
mditto1
Contributor III

Update:  I am able to boot U-boot from eMMC, interrupt to prevent booting of Android, and use these commands to boot Linux from the SD card:

 

fatload mmc 1:1 0x40480000 Image
fatload mmc 1:1 0x40470000 fsl-imx8mq-evk.dtb
setenv bootargs root=/dev/mmcblk1p2
booti 0x40480000 - 0x40470000

 

I don't know why the SD card cant be booted directly.

 

0 Kudos
Reply