iMX28 python3 via Yocto 1.6.11

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX28 python3 via Yocto 1.6.11

1,051件の閲覧回数
jfm
Contributor I

SYNOPSIS: A device based on the iMX28 requires updates to installed images created via Digi Embedded Yocto to include Python3 support. Specifically, I am starting with the Digi ConnectCard imx28 JumpStart board and its Yocto ecosystem.

Based on a literature review, the Digi support for this platform via the ConnectCard imx28 JumpStart board (i.e. ccardimx28js) appears to stopped in its DEY 1.6.11 release.

Working with that constraint, I have attempted unsuccessfully to include python3 in the Yocto. Is there a way to provide python3 support for ccardimx28js via DEY 1.6.11 (or any more modern DEY that may support this platform that I missed)?

Here's the first steps I tried.

I build by adding the following to my local.conf configuration file for DEY 1.6.11.

IMAGE_INSTALL_append = " python3"

I see the python 3.3.3 recipes being built, and these recipes appear to succeed. However, the final step to package them into the root file system fails.

Specifically, the log for the do_rootfs task shows the following errors. 

1 DEBUG: Executing python function rootfs_process_ignore
2 DEBUG: Python function rootfs_process_ignore finished
3 DEBUG: Executing python function rootfs_runtime_mapping
4 DEBUG: Python function rootfs_runtime_mapping finished
5 DEBUG: Executing python function do_rootfs
6 NOTE: configuring RPM platform settings
7 NOTE: configuring RPM system provides
8 NOTE: configuring RPM DB settings
9 NOTE: configuring Smart settings
10 NOTE: Note: adding Smart channel ccardimx28js (65)
11 NOTE: Note: adding Smart channel armv5te (60)
12 NOTE: Note: adding Smart channel all (55)
13 NOTE: adding Smart RPM DB channel
14 NOTE: Note: configuring RPM cross-install scriptlet_wrapper
15 NOTE: ###### Generate rootfs #######
16 NOTE: Executing '/home/x/workspace/ccardimx28js/tmp/sysroots/x86_64-linux/usr/bin/createrepo --update -q /home/x/workspace/ccardimx28js/tmp/deploy/rpm/all' ...
17 NOTE: Executing '/home/x/workspace/ccardimx28js/tmp/sysroots/x86_64-linux/usr/bin/createrepo --update -q /home/x/workspace/ccardimx28js/tmp/deploy/rpm/ccardimx28js' ...

<SNIP>

19 NOTE: Installing the following packages: packagegroup-core-ssh-dropbear packagegroup-dey-network run-postinsts smartpm packagegroup-dey-audio curl rpm packagegroup-dey-core python3
20 ERROR: python3 not found in the base feeds (ccardimx28js armv5te-mx28 armv5te armv5e armv5t armv5 armv4t armv4 arm noarch any all).

0 件の賞賛
返信
0 返答(返信)