MAPBGA footprint

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MAPBGA footprint

3,560 次查看
fluiss
Contributor I

Hi all,

I'm searching for any kind of information about the i.MX28 MAPBGA package. Datasheet says nothing about Paste Mask and Solder Mask expansion. As it is the first time I'm going to work with BGA I would like to pay special attention to every detail at the design stage.

Thx!!

Fernando

标签 (1)
0 项奖励
回复
4 回复数

3,039 次查看
ManuMartinez
Contributor I

I also have Altium: not Allegro. I asked a colleague who has Allegro which was the pad diameter of the balls.

Regards!

0 项奖励
回复

3,039 次查看
fluiss
Contributor I

Hi guys,

Thank you very much for the help. I use Altium and it has an importer of Allegro files but don't work if Allegro is not already installed in the computer and I can't take a look to the gerber files coming with the EVK. So very useful your comments!

cheers

0 项奖励
回复

3,039 次查看
fear_nada
Contributor I

hi i use

pad: 0.4mm for top and 0.5 for top mask

for wire 0.1

for via 0.2mm\0.4mm

0 项奖励
回复

3,039 次查看
ManuMartinez
Contributor I

Fernando,

as land pattern I've used the same value used in the EVK: 12mil. But I suspect that 13mil will be also appropiate.

With 4mil width/space for tracks and 8mil/16mil pad/hole for vias: the minimum reliable track/space for mask has been 0.08mm, in my case. DON'T FORGET TO COMPLETELY TENT  ALL THE VIAS UNDER THE BGA COMPONENTS. Regarding to the solder mask: I didn't put anything and my assembler did it for me.

My custom board works right. On any case I've planned to buy some IPC standards in order to be sure of what I'm doing on next designs.

Hope be helpful.

Manu.

0 项奖励
回复