How to use the CAN utilities with Qt4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use the CAN utilities with Qt4

2,318 次查看
AlexanderKelle1
Contributor II

I have a couple of questions about how to integrate the CAN utilities in Qt4. 

First, what are the configuration settings for the automotive board using a 500 kHz baud rate? 

Second, where are the header files that contain the CAN utilities prototypes so that I can call on the CAN functions in Qt? I know where the source source code for the CAN utilizes are and I found the script file that executes the command. However, there are no prototypes for the canecho, cansend, or canconfig functions. I can only call on these functions is through the terminal. Is there anyway that I can call on these functions through Qt? 

-Alexander Keller 

标记 (2)
0 项奖励
回复
3 回复数

2,210 次查看
Frias
Contributor V

on the Virtual disk provided in the training, if you open the qt-wspace on the Desktop, the demo project is in the: /home/lucid/Desktop/qt-wspace/UI_Save_1_10_12_Discrete_Sigs/UI_v2/

0 项奖励
回复

2,210 次查看
AlexanderKelle1
Contributor II

I am a little confused on what Qt demo you are talking about. The Qt demo on the PowerPoint slides does not use CAN messages or call on the class QProcess. Was there another Qt example that you gave us? If there is can you post it on the forum?

I looked at the powerpoint slide about configuring the CAN bus. I was wondering if the term BITTIME is the same has the baud rate?



Renato Frias said:

Hi Alexander,

On the Qt demo, it is just doing calling the CAN utilities, look for the "QProcess::execute" on some of the classes. This was only a quick and dirty way to implement it. You can study the utilities and integrate the code on your application.

As for the baud rate there is a slide on the ppt that talks about that, I'll ask Rebeca to comment on it.

Renato  

0 项奖励
回复

2,210 次查看
Frias
Contributor V

Hi Alexander,

On the Qt demo, it is just doing calling the CAN utilities, look for the "QProcess::execute" on some of the classes. This was only a quick and dirty way to implement it. You can study the utilities and integrate the code on your application.

As for the baud rate there is a slide on the ppt that talks about that, I'll ask Rebeca to comment on it.

Renato  

0 项奖励
回复