Lose static IP address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Lose static IP address

Jump to solution
4,638 Views
lqll
Contributor III

Hello

My environment is i.MX6Q sabreSD ,AR8031 phy,and OS is android 4.4.2.We use local network and we don't use wifi.We use RJ45 to connect a router.

When power on ,we give a static IP address to our board,.

pastedImage_0.png

but after several times of pluging/unpluging RJ45,the static IP address is changed to another.

pastedImage_1.png

Then we continue to plug/unplug sereral times,the IP address lost.

pastedImage_2.png

And I got this log from Android.

01-01 11:26:28.440: D/Ethernet(2614): Interface eth0 link up

01-01 11:26:30.840: D/ConnectivityService(2614): ConnectivityChange for ETHERNET: CONNECTED/CONNECTED

01-01 11:26:30.850: E/ConnectivityService(2614): Unexpected mtu value: android.net.EthernetDataTracker@41ccbbc0

01-01 11:26:30.860: D/Nat464Xlat(2614): requiresClat: netType=9, hasIPv4Address=true

01-01 11:26:33.870: D/Tethering(2614): MasterInitialState.processMessage what=3

01-01 11:26:33.870: D/CaptivePortalTracker(2614): NoActiveNetworkState{ when=0 what=1 obj=NetworkInfo: type: ETHERNET[], state: CONNECTED/CONNECTED, reason: (unspecified), extra: 12:25:30:3a:85:ae, roaming: false, failover: false, isAvailable: true, isConnectedToProvisioningNetwork: false target=com.android.internal.util.StateMachine$SmHandler }

01-01 11:26:33.870: D/CaptivePortalTracker(2614): NoActiveNetworkState not a wifi connectivity change, ignore

01-01 11:27:00.440: D/Ethernet(2614): Interface eth0 link down

01-01 11:27:00.640: D/CommandListener(2232): Clearing all IP addresses on eth0

01-01 11:27:00.650: D/Nat464Xlat(2614): requiresClat: netType=9, hasIPv4Address=false

01-01 11:27:00.650: D/ConnectivityService(2614): ConnectivityChange for ETHERNET: DISCONNECTED/DISCONNECTED

01-01 11:27:00.650: D/ConnectivityService(2614): tryFailover: set mActiveDefaultNetwork=-1, prevNetType=9

01-01 11:27:00.660: D/ConnectivityService(2614): Attempting to switch to mobile

01-01 11:27:00.660: D/ConnectivityService(2614): Attempting to switch to wifi

01-01 11:27:00.660: D/ConnectivityService(2614): Attempting to switch to BLUETOOTH_TETHER

01-01 11:27:00.660: D/Nat464Xlat(2614): requiresClat: netType=9, hasIPv4Address=false

01-01 11:27:03.670: D/Tethering(2614): MasterInitialState.processMessage what=3

01-01 11:27:03.670: D/CaptivePortalTracker(2614): NoActiveNetworkState{ when=0 what=1 obj=NetworkInfo: type: ETHERNET[], state: DISCONNECTED/DISCONNECTED, reason: (unspecified), extra: 12:25:30:3a:85:ae, roaming: false, failover: false, isAvailable: false, isConnectedToProvisioningNetwork: false target=com.android.internal.util.StateMachine$SmHandler }

01-01 11:27:03.670: D/CaptivePortalTracker(2614): NoActiveNetworkState not a wifi connectivity change, ignore

01-01 11:27:04.440: D/Ethernet(2614): Interface eth0 link up

01-01 11:27:06.840: D/ConnectivityService(2614): ConnectivityChange for ETHERNET: CONNECTED/CONNECTED

01-01 11:27:06.850: E/ConnectivityService(2614): Unexpected mtu value: android.net.EthernetDataTracker@41ccbbc0

01-01 11:27:06.860: D/Nat464Xlat(2614): requiresClat: netType=9, hasIPv4Address=true

01-01 11:27:09.870: D/CaptivePortalTracker(2614): NoActiveNetworkState{ when=0 what=1 obj=NetworkInfo: type: ETHERNET[], state: CONNECTED/CONNECTED, reason: (unspecified), extra: 12:25:30:3a:85:ae, roaming: false, failover: false, isAvailable: true, isConnectedToProvisioningNetwork: false target=com.android.internal.util.StateMachine$SmHandler }

01-01 11:27:09.870: D/CaptivePortalTracker(2614): NoActiveNetworkState not a wifi connectivity change, ignore

01-01 11:27:09.870: D/Tethering(2614): MasterInitialState.processMessage what=3

01-01 11:27:15.290: D/dalvikvm(3120): GC_FOR_ALLOC freed 512K, 18% free 2780K/3372K, paused 12ms, total 12ms

Labels (3)
0 Kudos
Reply
1 Solution
3,994 Views
lqll
Contributor III

use dhcpcd like below can solve this problem

dhcpcd -S ip_address=10.0.0.135 -S rounters=10.0.0.1 -S subnet_mask=255.255.255 eth0

View solution in original post

0 Kudos
Reply
3 Replies
3,995 Views
lqll
Contributor III

use dhcpcd like below can solve this problem

dhcpcd -S ip_address=10.0.0.135 -S rounters=10.0.0.1 -S subnet_mask=255.255.255 eth0

0 Kudos
Reply
3,994 Views
igorpadykov
NXP Employee
NXP Employee

Hi lkl

one can look at uboot parameters

http://www.denx.de/wiki/view/DULG/LinuxKernelArgs

http://serverfault.com/questions/445296/is-there-a-linux-kernel-boot-parameter-to-configure-an-ipv6-...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,994 Views
lqll
Contributor III

Hi igor

Thanks for your reply.

My problem is no relation to uboot.No matter what IP address setted in uboot,I will change IP address in kernel, and this is my command:

ifconfig eth0 10.0.0.135 netmask 255.255.255.0

But after I plug and unplug RJ45 many times,My static IP address auto change to 10.0.0.32,then I continue to plug and unplug RJ45 many times,the IP address is gone.

During this test,I didn't reboot board or reset IP address,and didn't run any APP.

0 Kudos
Reply