Loop back of Display output data to CSI inputs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Loop back of Display output data to CSI inputs

1,542件の閲覧回数
harishs
Contributor I

Hi

We are using IMX6 Quad based COM for one of our end application,need info on whether it is possible to loop back LVDS Display or MIPI DSI outputs from the processor to MIPI CSI for validation of CSI interaface in our end application with some test data.

Need also some first hand information on data format compatibility between these interfaces.

ラベル(1)
0 件の賞賛
返信
1 返信

1,370件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Harish

seems lvds is not compatible with mipi-dphy,

both mipi dsi and csi have mipi-dphy and can be connected together.

However timings and protocols are different so seems this also not possible.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信