Which IDE?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which IDE?

2,385 Views
adelantesey
Contributor IV

Dear My friends,

could any one suggest an IDE for debugging M4 of iMx6soloX, i want an IED based on Linux (dist: ubuntu)

of course the best is eclips but i'm not sure if it can debug! if it can, which tool should i use? (i mean like u-link from keil)

Labels (1)
0 Kudos
Reply
3 Replies

2,236 Views
igorpadykov
NXP Employee
NXP Employee

Hi Adelante

please check AN5229 ARM DS-5 Development Studio Debug i.MX6UL-EVK
http://www.nxp.com/assets/documents/data/en/application-notes/AN5229.pdf
AN5127 How to Run the MQX™ RTOS on Various RAM Memories for i.MX 6SoloX
http://www.nxp.com/assets/documents/data/en/application-notes/AN5127.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,236 Views
adelantesey
Contributor IV

Dear Igor,

sorry. i got it.

thanks again.

regards

0 Kudos
Reply

2,236 Views
adelantesey
Contributor IV

Dear Igor,

thanks for the answer, but i need a tool on linux (ubuntu)

best regards

0 Kudos
Reply