Loop back of Display output data to CSI inputs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Loop back of Display output data to CSI inputs

2,041 次查看
harishs
Contributor I

Hi

We are using IMX6 Quad based COM for one of our end application,need info on whether it is possible to loop back LVDS Display or MIPI DSI outputs from the processor to MIPI CSI for validation of CSI interaface in our end application with some test data.

Need also some first hand information on data format compatibility between these interfaces.

标签 (1)
0 项奖励
回复
1 回复

1,869 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Harish

seems lvds is not compatible with mipi-dphy,

both mipi dsi and csi have mipi-dphy and can be connected together.

However timings and protocols are different so seems this also not possible.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复