Linux.bin (Boot Linux without U-boot)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Linux.bin (Boot Linux without U-boot)

1,869 次查看
ailtonlopes
Contributor III

Hi, 

Im trying to create a .bin file for linux including the zImage and the Device tree and filesystem for the Imx6QSD following a tutorial made fo the Zedboard and i used the zImage and .dtb created using buildroot, my question is what are the pre-boot steps necessary to boot linux on the imx6QSD board.

At the moment im passing to the kernel when calling it the address of the .dtb and the Machine ID. 

btw the .bin is necessary to use it as the non-secure guest of an trustzone assisted hypervisor.

Kind Regards, 

Ailton Lopes

标签 (3)
0 项奖励
回复
1 回复

1,701 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 项奖励
回复