Linux.bin (Boot Linux without U-boot)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux.bin (Boot Linux without U-boot)

1,866件の閲覧回数
ailtonlopes
Contributor III

Hi, 

Im trying to create a .bin file for linux including the zImage and the Device tree and filesystem for the Imx6QSD following a tutorial made fo the Zedboard and i used the zImage and .dtb created using buildroot, my question is what are the pre-boot steps necessary to boot linux on the imx6QSD board.

At the moment im passing to the kernel when calling it the address of the .dtb and the Machine ID. 

btw the .bin is necessary to use it as the non-secure guest of an trustzone assisted hypervisor.

Kind Regards, 

Ailton Lopes

ラベル(3)
0 件の賞賛
返信
1 返信

1,698件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信