Layout suggestion for PF100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Layout suggestion for PF100

910 Views
aabhishekoct18
Contributor III

Hi Team 

As  per  application notes  AN4717  pin no 48 of  PF100  is  GND  reference it should  be  keep away from high switching GND  reference  path   

pastedImage_1.png

But in layout  file  it is  connected  to GND  EP. Should  i caonnect this with GND  EP  or  connect to GND plane 

through separate via.

pastedImage_2.png

Labels (1)
0 Kudos
Reply
1 Reply

845 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abhishek

example of connection of pin no 48 of  PF100 can be found in  iMX6Q-SABRE-SDB-DESIGNFILES

Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 6Quad (i.MX 6Dual emu...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply