LTIB compile

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LTIB compile

Jump to solution
2,985 Views
carmilili
Contributor III

When I compile LTIB , I need the below choice.Who can tell me the difference between six choice.The more detailed the better.Thank you.

peiz.png

Labels (2)
0 Kudos
Reply
1 Solution
2,737 Views
jimmychan
NXP TechSupport
NXP TechSupport

Min. profile is a small and basic root filesystem contains busybox, imx test, imx lib, etc. The building time is short around 30mins.

FSL gnome profile is a GNOME GUI example. It contains many packages and it will start a GNOME GUI when the board start up. The building time is very long ~4-5hrs.

You can compare the .profile files of each profile under <ltib>/config/platform/imx/.

e.g. min.profile is Min. profile,  release_gnome.profile is GNOME profile.

After you selected the profile,  you can select/deselect the package again in the "Package List" in LTIB configuration.

View solution in original post

0 Kudos
Reply
3 Replies
2,738 Views
jimmychan
NXP TechSupport
NXP TechSupport

Min. profile is a small and basic root filesystem contains busybox, imx test, imx lib, etc. The building time is short around 30mins.

FSL gnome profile is a GNOME GUI example. It contains many packages and it will start a GNOME GUI when the board start up. The building time is very long ~4-5hrs.

You can compare the .profile files of each profile under <ltib>/config/platform/imx/.

e.g. min.profile is Min. profile,  release_gnome.profile is GNOME profile.

After you selected the profile,  you can select/deselect the package again in the "Package List" in LTIB configuration.

0 Kudos
Reply
2,737 Views
carmilili
Contributor III

Thank you for your reply.I get what I want to know.

0 Kudos
Reply
2,737 Views
LeonardoSandova
Specialist I

A profile can be seen as a set of packages, most of them are installed on the rootfs. In order to see differences between two profiles, you can compare the config directories. In other words, create to ltib folders, in one select the min profile and in other the gnome, then compare the config folders of each one....

Leo

0 Kudos
Reply