LTIB compile

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,973件の閲覧回数
carmilili
Contributor III

When I compile LTIB , I need the below choice.Who can tell me the difference between six choice.The more detailed the better.Thank you.

peiz.png

ラベル(2)
0 件の賞賛
返信
1 解決策
2,725件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Min. profile is a small and basic root filesystem contains busybox, imx test, imx lib, etc. The building time is short around 30mins.

FSL gnome profile is a GNOME GUI example. It contains many packages and it will start a GNOME GUI when the board start up. The building time is very long ~4-5hrs.

You can compare the .profile files of each profile under <ltib>/config/platform/imx/.

e.g. min.profile is Min. profile,  release_gnome.profile is GNOME profile.

After you selected the profile,  you can select/deselect the package again in the "Package List" in LTIB configuration.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,726件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Min. profile is a small and basic root filesystem contains busybox, imx test, imx lib, etc. The building time is short around 30mins.

FSL gnome profile is a GNOME GUI example. It contains many packages and it will start a GNOME GUI when the board start up. The building time is very long ~4-5hrs.

You can compare the .profile files of each profile under <ltib>/config/platform/imx/.

e.g. min.profile is Min. profile,  release_gnome.profile is GNOME profile.

After you selected the profile,  you can select/deselect the package again in the "Package List" in LTIB configuration.

0 件の賞賛
返信
2,725件の閲覧回数
carmilili
Contributor III

Thank you for your reply.I get what I want to know.

0 件の賞賛
返信
2,725件の閲覧回数
LeonardoSandova
Specialist I

A profile can be seen as a set of packages, most of them are installed on the rootfs. In order to see differences between two profiles, you can compare the config directories. In other words, create to ltib folders, in one select the min profile and in other the gnome, then compare the config folders of each one....

Leo

0 件の賞賛
返信