LTIB build fails

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LTIB build fails

2,504 次查看
eugenesolo
Contributor II

After i fixed some strange errors in gzipped sources (flex and others), configured kernel and so on, ./ltib  (from 4.1.0 source) still fails to build base_libs:

-----

cp -a /opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-gcc//include/c++ /home/eugene/LTIB/ltib/tmp/base_libs//opt/freescale/rootfs/arm/usr/include

cp: cannot stat '/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-gcc//include/c++': Not a directory

error: Bad exit status from /home/eugene/LTIB/ltib/tmp/rpm-tmp.3188 (%install)

    Bad exit status from /home/eugene/LTIB/ltib/tmp/rpm-tmp.3188 (%install)

RPM build errors:

Failed building base_libs

Build time for base_libs: 1 seconds

f_buildrpms() returned an error, exiting

-----

Of course, "/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-gcc//include/c++" is not a directory, it doesn't even exist!

I guess, this is just a typo in some of the scripts, but i cant figure where and what.

标签 (2)
6 回复数

2,042 次查看
LeonardoSandova
Specialist I

What were the fixes you did? please share them as patches. Can you just compile base_libs ?

./ltib -m prep -p base_libs
./ltib -m scbuild -p base_libs
./ltib -m scdeploy -p base_libs

0 项奖励
回复

2,042 次查看
eugenesolo
Contributor II

./ltib -m prep -p base_libs

     did well, but

./ltib -m scbuild -p base_libs

     died instantly because of error:

/home/eugene/LTIB/ltib/tmp/rpm-tmp.84041: 38: /home/eugene/LTIB/ltib/tmp/rpm-tmp.84041: 1: not found

first patch was already deployed by somebody, I'd found it later (something about "gets", don't remember :smileyhappy:), second was an absolute path to sys/types.h (which is not correct for my system) and others was just a missed system files (texinfo, etc.)

0 项奖励
回复

2,042 次查看
LeonardoSandova
Specialist I

Not sure. Please try cleaning your package (-m clean -p ...) and try again. I have compiled base_libs without problems :smileysad: . have you changed something on the spec?

Loe

0 项奖励
回复

2,042 次查看
eugenesolo
Contributor II

no, specs wasn't edited at all, just installed missing packages (my system is Ubintu 13.10 upgraded from live CD 13.04) and fixed some typo

./ltib -m clean -p base_libs

base_libs is not installed

(and this is understandable - base_libs is not installed because it is not compiled)

0 项奖励
回复

2,042 次查看
LeonardoSandova
Specialist I

I see. There are some patches out there in order to use LTIB with Ubuntu 13.X. I am not sure if your problem is related to this version but either apply patches or move to an older Ubuntu version (12.04 works like charm)

0 项奖励
回复

2,042 次查看
konstantinkoval
Contributor II

Unfortunately, I have the same problem with LTIB on my Fedora 19 (x86_64). I have tried to solve it by creating the symbolic link to /c++ directory from /gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12 (I have found it there by "mc" search). After that building process continued, but I have got another error with libc.so.6 wich doesn't exist in /opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/lib directory (Yep! It's true, this directory contain about 5 files only...). Could someone help me? I would be grateful for any advices!

0 项奖励
回复