LTIB build fails

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LTIB build fails

2,550 Views
eugenesolo
Contributor II

After i fixed some strange errors in gzipped sources (flex and others), configured kernel and so on, ./ltib  (from 4.1.0 source) still fails to build base_libs:

-----

cp -a /opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-gcc//include/c++ /home/eugene/LTIB/ltib/tmp/base_libs//opt/freescale/rootfs/arm/usr/include

cp: cannot stat '/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-gcc//include/c++': Not a directory

error: Bad exit status from /home/eugene/LTIB/ltib/tmp/rpm-tmp.3188 (%install)

    Bad exit status from /home/eugene/LTIB/ltib/tmp/rpm-tmp.3188 (%install)

RPM build errors:

Failed building base_libs

Build time for base_libs: 1 seconds

f_buildrpms() returned an error, exiting

-----

Of course, "/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-gcc//include/c++" is not a directory, it doesn't even exist!

I guess, this is just a typo in some of the scripts, but i cant figure where and what.

Labels (2)
6 Replies

2,088 Views
LeonardoSandova
Specialist I

What were the fixes you did? please share them as patches. Can you just compile base_libs ?

./ltib -m prep -p base_libs
./ltib -m scbuild -p base_libs
./ltib -m scdeploy -p base_libs

0 Kudos
Reply

2,088 Views
eugenesolo
Contributor II

./ltib -m prep -p base_libs

     did well, but

./ltib -m scbuild -p base_libs

     died instantly because of error:

/home/eugene/LTIB/ltib/tmp/rpm-tmp.84041: 38: /home/eugene/LTIB/ltib/tmp/rpm-tmp.84041: 1: not found

first patch was already deployed by somebody, I'd found it later (something about "gets", don't remember :smileyhappy:), second was an absolute path to sys/types.h (which is not correct for my system) and others was just a missed system files (texinfo, etc.)

0 Kudos
Reply

2,088 Views
LeonardoSandova
Specialist I

Not sure. Please try cleaning your package (-m clean -p ...) and try again. I have compiled base_libs without problems :smileysad: . have you changed something on the spec?

Loe

0 Kudos
Reply

2,088 Views
eugenesolo
Contributor II

no, specs wasn't edited at all, just installed missing packages (my system is Ubintu 13.10 upgraded from live CD 13.04) and fixed some typo

./ltib -m clean -p base_libs

base_libs is not installed

(and this is understandable - base_libs is not installed because it is not compiled)

0 Kudos
Reply

2,088 Views
LeonardoSandova
Specialist I

I see. There are some patches out there in order to use LTIB with Ubuntu 13.X. I am not sure if your problem is related to this version but either apply patches or move to an older Ubuntu version (12.04 works like charm)

0 Kudos
Reply

2,088 Views
konstantinkoval
Contributor II

Unfortunately, I have the same problem with LTIB on my Fedora 19 (x86_64). I have tried to solve it by creating the symbolic link to /c++ directory from /gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12 (I have found it there by "mc" search). After that building process continued, but I have got another error with libc.so.6 wich doesn't exist in /opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/lib directory (Yep! It's true, this directory contain about 5 files only...). Could someone help me? I would be grateful for any advices!

0 Kudos
Reply