LTIB ::: Problem with the Kernel Image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LTIB ::: Problem with the Kernel Image

9,146 Views
KrishnaPavan
Contributor II

U-Boot 2009.08 (Sep 22 2011 - 18:55:30)                                                                       

CPU:   Freescale i.MX51 family 3.0V at 800 MHz
mx51 pll1: 800MHz
mx51 pll2: 665MHz
mx51 pll3: 216MHz
ipg clock     : 66500000Hz
ipg per clock : 665000000Hz
uart clock    : 54000000Hz
cspi clock    : 54000000Hz
axi_a clock   : 166250000Hz
axi_b clock   : 133000000Hz
emi_slow clock: 83125000Hz
ddr clock     : 166250000Hz
esdhc clock   : 216000000Hz
Board: MX51 BABBAGE 3.0 [POR]
Boot Device: MMC
I2C:   ready
DRAM:  512 MB
MMC:   FSL_ESDHC: 0, FSL_ESDHC: 1
*** Warning - bad CRC or MMC, using default environment

In:    serial
Out:   serial
Err:   serial
PMIC Mode: SPI
Net:   got MAC address from IIM: 00:04:9f:02:09:65
FEC0 [PRIME]
Hit any key to stop autoboot:  0
*** ERROR: `serverip' not set
Wrong Image Format for bootm command
ERROR: can't get kernel image!
BBG U-Boot >

 

Later on nothing can be typed nor anything could not be entered.

 

I loaded the kernel image from the /ltib/rootfs/boot.......uImage properly only, even then i could not get the result.

Labels (1)
Tags (2)
0 Kudos
Reply
22 Replies

8,356 Views
KrishnaPavan
Contributor II

The COM Port does not work proper some times,

So unable to communicate...... Anyway USB-to-Serial has been a better solution

0 Kudos
Reply

8,356 Views
KrishnaPavan
Contributor II

Hi,        SOLVED Daiane

 

To get out of the error

I have replaced the Serial[RS232] Cable with a new serial cable,  even then it did not work,

So, I used a USB to SERIAL Cable, and it WORKED.

 

However, tests showed that both my Serial Cable, and modem card are not working properly.

Note :: All the Drivers are installed.

 

So, Lesson learnt is that Sometimes we need to check our hardware also.

Hardware that used to work perfectly went wrong and I could not recognize that it went wrong.

 

Coming to the highlighted lines, after using USB2Serial, I changed the environment variables.

The reason for that error is that, the board is trying to boot from the nfs instead of MMC/SD, However I had to make some change in the settings finally to get the board to boot from.

 

Thanks to Vladan Jovanovic, and especially Daiane  Angolini.         Regards    ::    Krishna Pavan

0 Kudos
Reply

8,356 Views
daiane_angolini
NXP Employee
NXP Employee

hum.

 

* your u-boot version is the right one

* your hardware is ok

* your SDCard hardware is ok

* your procedure to build the sdcard is ok

 the only missing thing I can imagine now is the u-boot environment variable.

 

Your u-boot tells it's Board: MX51 BABBAGE 3.0 [POR] Is your hardware TO 3.0?

0 Kudos
Reply

8,356 Views
KrishnaPavan
Contributor II

Hi Daiane..,

 

The procedure thats given is the same as that in the Linux_BSP_Users_Guide_for iMX51 Daiane ..

The u-boot version is proper

The procedure is correct, No Doubt about it.

I am getting everything changed right from  Cable and the connecting modem. I have already changed a new SD Card.

I Hope to get some response...          Krishna Pavan

0 Kudos
Reply

8,356 Views
daiane_angolini
NXP Employee
NXP Employee

I'm confused.

 

Why you're following i.MX_3D_Stack Users Guide if your board is iMX51?

 

Are you sure you're using the right u-boot version for your board?

0 Kudos
Reply

8,356 Views
KrishnaPavan
Contributor II

The Hardware is O.K.

I have tried with two new SanDisk 4 GB SD Cards.

I have tried by making the partitions as suggested by you and that from the i.MX_3D_Stack Users Guide from the freescale documents downloaded from freescale.com.

 

Even then the same error exists.....

*** Warning - bad CRC or MMC, using default environment

The error line is found in env_mmc.c file ltib/rpm/BUILD/u-boot-2009.08/common/env_mmc.c

There is some problem with the CRC Checks... I am trying to solve this issue..and am expecting some help...


0 Kudos
Reply

8,356 Views
daiane_angolini
NXP Employee
NXP Employee

Does anything works on your board? I mean, is your hardware OK?

 

Is your sdcard ok?

0 Kudos
Reply

8,356 Views
KrishnaPavan
Contributor II

sudo dd if=u-boot.bin of=/dev/sdb bs=512 && sync && sync                     
sudo dd if=uImage of=/dev/sdb bs=512 seek=2048 && sync && sync               

sudo fdisk /dev/sdb
            u           [switch the unit to sectors instead of cylinders]
            d           [repeat this until no partition is reported by the ‘p’ command ]
            n           [create a new partition]
            p           [create a primary partition]
            1           [the first partition]
            8192        [starting at offset sector #8192, i.e. 4MB, which leaves enough space for the kernel, the boot loader and its configuration data]
            <enter>     [using the default value will create a partition that spans to the last sector of the medium]
            w           [ this writes the partition table to the medium and fdisk exits]

sudo mkfs.ext3 /dev/sdb1

mkdir /home/user/mountpoint
cd /home/user/ltib/ltib/rootfs

sudo mount /dev/sdb1 /home/user/mountpoint

sudo cp -rpa [A-z]* /home/user/mountpoint

sudo umount /home/user/mountpoint

 

These are the command lines.

 

I have gone through the link http://imxcommunity.org/group/ltib/forum/topics/where-are-these-images-in-ltib?commentId=4103961%3AC... and saw the pic, and allocation of space, even the i could not get the result.

0 Kudos
Reply

8,356 Views
ManotSwasdee
NXP Employee
NXP Employee

Try a brand New SD Card. Partition the card with Linux EXT4 format with 15MB reserved for u-boot and kernel. 

Install the uboot with 'sudo dd if=<your u-boot such as u-boot.bin from rootfs/boot directory> of=/dev/sdb bs=512 seek=1 skip=1'.  I assume that your u-boot.bin is padded and the SD Card reader is mounted as '/dev/sdb'.  Then try to see if it works better.  Your card may be slow.  Use good SD Card such as SanDisk with Class 2 or higher.

0 Kudos
Reply

8,356 Views
daiane_angolini
NXP Employee
NXP Employee

I´ve never seem this behavior before.

 

Can you share command line you used to copy u-boot?

 

When I want to clear the first memory of a sdcard I copy a big image to sdcard and remake everything else.

Something like:

sudo dd if=some_huge_file of=/dev/sdbX

and then gparted stuff (rebuilt MBR and partitions)

and then copy uboot again.

 

it clears uboot variables too.

0 Kudos
Reply

8,356 Views
KrishnaPavan
Contributor II

Yeah! I have tried to program that section of the memory also many times...........

I tried to experiment with the partitions also.......

finally ended up with the correct procedure.............

But with the unresponsive prompt

0 Kudos
Reply

8,356 Views
Don_ng
Contributor I
Try erasing that section of memory before you program it.  I've run into this and erasing it and reprogramming seems to clear it up.
0 Kudos
Reply

8,356 Views
KrishnaPavan
Contributor II

I am using linux ubuntu 10.04.

 

I have formatted my hard disk and installed linux on my system and am doing all this stuff related to i.MX5X EVK board.....

No Virtual Machine is used......

0 Kudos
Reply

8,355 Views
KrishnaPavan
Contributor II

No Problem with the Cable, thats for sure I have got it double checked.

 

The point of concern is

              my bootloader u-boot.bin is 153 KB, How to place it in the SD card slot and how to avoid the CRC error,

 

My bootloader is occupying more space where it cannot be read any more because it exceeded the space/ has started in a wrong place.

 

How to resolve this...

The error message *** Warning - bad CRC or MMC, using default environment

is found in /ltib/rpm/BUILD/u-boot.29.08/common/env_mmc.c

 

So, then there should be a connection....... Thats what I have been thinking.

0 Kudos
Reply

8,356 Views
daiane_angolini
NXP Employee
NXP Employee

double check your minicom (or screen) configuration:

http://www.imxdev.org/wiki/index.php?title=All_Boards_Serial_Console

 

make sure you´re using the right serial device.

 

Are you using VMWare image?????????????????????

0 Kudos
Reply

8,356 Views
VladanJovanovic
NXP Employee
NXP Employee

Hm, looks good. Did you try with another serial cable? In the end, it might be there's something wrong with the board you have, might we worth checking signals with oscilloscope if you have that or then replace the board...

It's very unusual if you can't get any serial communication with u-boot.

 

What if you just type "printenv" and press enter? (not sure if local echo needs to be enabled, but I don't think so...)

0 Kudos
Reply

8,356 Views
KrishnaPavan
Contributor II
606-serial_snap.png
0 Kudos
Reply

8,356 Views
VladanJovanovic
NXP Employee
NXP Employee

there's something wrong with your serial port setup or cable. Can you post a snapshot of your serial console settings in PC you're using?

0 Kudos
Reply

8,356 Views
KrishnaPavan
Contributor II

I amnot even able to interrupt to stop

 

Hit any key to STOP autoboot: in x seconds

I tried many times but could not interrupt.

I dont know how to resolve this?

I have been trying this for long time, yet could not get any output in my favour...........

0 Kudos
Reply

8,356 Views
VladanJovanovic
NXP Employee
NXP Employee
bad CRC... error is nothing special, it just says that in area allocated to store u-boot settings there is no data, so default setup will be used. You should still be able to communicate with u-boot. What about if you interrupt u-boot before it tries to load kernel?
0 Kudos
Reply