iMX53 QSB 640x480?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX53 QSB 640x480?

966 Views
yvan
Contributor II

Hello,

 

I'm trying to use a 640x480 LVDS screen on my mx53QSB.

So I added 

         /* 640x480 @ 60 Hz, 31.5 kHz hsync */

        { "VGA", 60, 640, 480, 39721,

        40, 24,

        32, 11,

        96, 2,

         0,

        FB_VMODE_NONINTERLACED,

        0,},

in video_modes[] of arch/arm/mach-mx5/mx53_loco.c

recompiled...

 

Then I changed my uBoot env

lvds=mxcdi0fb:RGB666,VGA ldb

instead of

lvds=mxcdi0fb:RGB666,XGA ldb

 

And... I've got nothing on the screen

 

Note : When using XGA the screen is working (with a cropped image of course)

 

What am I missing? 

Tags (1)
0 Kudos
2 Replies

733 Views
LilyZhang
Contributor I

Yes. Please ensure you also add relative mode into drivers/video/mxc/ldb.c.

Please also check the clock configurations in ldb.c and ensure it can support your panel

0 Kudos

733 Views
yvan
Contributor II

Ok! just found it!

We also need to add this new mode in :

drivers/video/mxc/ldb.c

0 Kudos