LTIB Config Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LTIB Config Issue

2,248 Views
ManojCR
Contributor I

Hi,

 

We are trying to enable USB Webcam .For that we first installed LTIB and then when we give ./LTIB -c command it gives the following error.

 

Error 1
make[2]: Leaving directory `/tmp/rpm-ubuntu/BUILD/rpm-4.0.4/tools'
make[1]: *** [all-recursive] Error 1
make[1]: Leaving directory `/tmp/rpm-ubuntu/BUILD/rpm-4.0.4'
make: *** [all-recursive-am] Error 2
error: Bad exit status from /media/disk/L2.6.31_10.07.11_ER_source/y/ltib/tmp/rpm-tmp.54676 (%build)


RPM build errors:
    Bad exit status from /media/disk/L2.6.31_10.07.11_ER_source/y/ltib/tmp/rpm-tmp.54676 (%build)
Build time for rpm-fs: 1435 seconds

Failed building rpm-fs
could not glob rpm in: /tmp/rpm-ubuntu/RPMS/armv7l/rpm-fs-* at ./ltib line 2408.
traceback:
 main::check_rpm_setup:2408
  main::host_checks:1423
   main:542


Started: Tue Oct 26 06:36:08 2010
Ended:   Tue Oct 26 07:00:08 2010
Elapsed: 1440 seconds

These packages failed to build:
rpm-fs

Build Failed

 

 

Please let me know the reason for the error.

 

Am also attaching the log file with this.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,765 Views
SpringZhang
Contributor II

Maybe it's late to reply, just some comments:


From the log, librpmio lib is missing:
../rpmio/.libs/librpmio.so: undefined reference to `mp32addmul'
../rpmio/.libs/librpmio.so: undefined reference to `mp32setmul'
collect2: ld returned 1 exit status
make[2]: *** [dump] Error 1

if you're on Ubuntu, try to install librpmio deb by: "sudo apt-get install librpmio0", it may help. Other related librpm* packages:

librpm0       librpm1-dev   librpm-dbg 
librpm0-dev   librpmbuild0  librpm-dev   

0 Kudos
Reply