LTIB Build Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LTIB Build Error

2,312 Views
arunachalamrama
Contributor III

I am able to build L3.0.35_4.1.0 on Ubuntu 14.04.

After applying Multimedia Codec, I get error given below.

I tried different solutions suggested in freescale community and other websites. Problem is still there.

Please let me know if this can be solved or another Linux version with Multimedia Codec (gstreamer) support.

Regards,

Arun

Processing: fsl-alsa-plugins

==============================

Build path taken because: no prebuilt rpm,

Testing network connectivity

OK GPP:

Try fsl-alsa-plugins-1.0.25.tar.gz.md5 from the GPP

http://bitshrine.org/gpp/fsl-alsa-plugins-1.0.25.tar.gz.md5:

02:03:28 ERROR 404: Not Found.

Try fsl-alsa-plugins-1.0.25.tar.gz from the GPP

http://bitshrine.org/gpp/fsl-alsa-plugins-1.0.25.tar.gz:

02:03:28 ERROR 404: Not Found.

Can't get: fsl-alsa-plugins-1.0.25.tar.gz at ./ltib line 802.

f_buildrpms() returned an error, exiting

traceback:

main:572

Started: Thu Apr 21 02:00:05 2016

Ended:   Thu Apr 21 02:03:28 2016

Elapsed: 203 seconds

These packages failed to build:

fsl-alsa-plugins

Build Failed

Exiting on error or interrupt

Labels (3)
0 Kudos
Reply
3 Replies

2,056 Views
jimmychan
NXP TechSupport
NXP TechSupport

I would suggest you to use Yocto BSP. LTIB is old and will not have any new BSP release.

0 Kudos
Reply

2,056 Views
arunachalamrama
Contributor III

Thanks, jimmychan, for the  update and suggestion.

Please suggest Yocto version with gstreamer support.

Arun

0 Kudos
Reply

2,056 Views
arunachalamrama
Contributor III

Downloaded Linux source and MM Codec source from this link: i.MX 6 Q/D/DL/S L3.0.35_4.1.0 GA release

0 Kudos
Reply