LTIB Build Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LTIB Build Error

2,501件の閲覧回数
arunachalamrama
Contributor III

I am able to build L3.0.35_4.1.0 on Ubuntu 14.04.

After applying Multimedia Codec, I get error given below.

I tried different solutions suggested in freescale community and other websites. Problem is still there.

Please let me know if this can be solved or another Linux version with Multimedia Codec (gstreamer) support.

Regards,

Arun

Processing: fsl-alsa-plugins

==============================

Build path taken because: no prebuilt rpm,

Testing network connectivity

OK GPP:

Try fsl-alsa-plugins-1.0.25.tar.gz.md5 from the GPP

http://bitshrine.org/gpp/fsl-alsa-plugins-1.0.25.tar.gz.md5:

02:03:28 ERROR 404: Not Found.

Try fsl-alsa-plugins-1.0.25.tar.gz from the GPP

http://bitshrine.org/gpp/fsl-alsa-plugins-1.0.25.tar.gz:

02:03:28 ERROR 404: Not Found.

Can't get: fsl-alsa-plugins-1.0.25.tar.gz at ./ltib line 802.

f_buildrpms() returned an error, exiting

traceback:

main:572

Started: Thu Apr 21 02:00:05 2016

Ended:   Thu Apr 21 02:03:28 2016

Elapsed: 203 seconds

These packages failed to build:

fsl-alsa-plugins

Build Failed

Exiting on error or interrupt

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

2,245件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I would suggest you to use Yocto BSP. LTIB is old and will not have any new BSP release.

0 件の賞賛
返信

2,245件の閲覧回数
arunachalamrama
Contributor III

Thanks, jimmychan, for the  update and suggestion.

Please suggest Yocto version with gstreamer support.

Arun

0 件の賞賛
返信

2,245件の閲覧回数
arunachalamrama
Contributor III

Downloaded Linux source and MM Codec source from this link: i.MX 6 Q/D/DL/S L3.0.35_4.1.0 GA release

0 件の賞賛
返信