LPDDR4 Capacity for IMX8M Mini

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPDDR4 Capacity for IMX8M Mini

跳至解决方案
9,160 次查看
haryanl
Contributor IV

Hello,

I'm planning to change 2GB LPDDR4 to 4GB for the IMX8M Mini Quad board.

Or change 2GB to 1/2/4 / 8GB
→Is there a problem, when not changing the hardware design?

Many Thanks.

1 解答
8,520 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

The 4GB can work. And for 8GB DRAM, lower 3GB can be accessed by all the modules, higher 5GB is A53 CPU only.

Hope this can do help for you.

在原帖中查看解决方案

13 回复数
8,521 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

The 4GB can work. And for 8GB DRAM, lower 3GB can be accessed by all the modules, higher 5GB is A53 CPU only.

Hope this can do help for you.

8,238 次查看
NATHANKLOGIC
Contributor III

Hi

Is the higher 5GB available to any configuration of the A53 or only when using a Quad-A53?  The following note is in the i.MX 8M Mini RM that specifically states the "Quad-A53".  It is not clear to me why it would be the Quad configuration only.

NATHANKLOGIC_0-1616085320830.png

Thanks!

0 项奖励
回复
8,520 次查看
haryanl
Contributor IV

Hi Rita Wang,

(I decided to use 2GB LPDDR4)
But, Can you show me, can I use LPDDR4 500MB for mini IMX8M

I just want more information
Thank you very much

0 项奖励
回复
8,520 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

If you are using the 2GB LPDDR4, you can refer to our reference design.

0 项奖励
回复
8,520 次查看
haryanl
Contributor IV

yes, that's right, I did refer to the reference circuit.
But my superior wants to confirm the above information
Please confirm to me

Many Thanks

0 项奖励
回复
8,520 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Confirm "LPDDR4 500MB for mini IMX8M"? I am confused

8,520 次查看
haryanl
Contributor IV

yes, is it

0 项奖励
回复
8,519 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

If you do not use the GPU,VPU, the 512MB can work. But do not recommend you to use. You can use 2GB as our reference design.

0 项奖励
回复
8,520 次查看
haryanl
Contributor IV

Thanks for your support
I used 2GB LPDDR4 and it worked properly

0 项奖励
回复
8,519 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Good~~

0 项奖励
回复
8,519 次查看
haryanl
Contributor IV

Thank you for your support

0 项奖励
回复
8,520 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

I need to confirm it for you and then give you reply.

Have a nice day

Rita

0 项奖励
回复
8,520 次查看
haryanl
Contributor IV

Thank you
I would appreciate your favor

0 项奖励
回复