Using GPU on IMX-8qxp for CNN Inference

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using GPU on IMX-8qxp for CNN Inference

1,458件の閲覧回数
parag_jain
Contributor I

Context :

I would like to inference my CNN model on IMX-8qxp unit. As your website states, inference is supported on Vulkan GPU on IMX-8qxp through eIQ for ARM-NN & TF-Lite models(https://www.nxp.com/docs/en/fact-sheet/EIQ-FS.pdf )[Page-2] . Following are the related questions. 

Questions :

1) IMX-8qxp has 1x4-shader Vulkan GPU. Can we access this GPU using latest eIQ package for CNN model inference? 
2) If yes, would you please share some reference documents? 
3) If GPU based CNN inference is supported, can we use eIQ as stand-alone module or does it BSP to be rebuilt? 
4) GpuAcc flag in ARM-NN supports only Mali-based GPU. Can you please point me to a sample C++ testapp in which eIQ is used for inference on Vulkan GPU?

タグ(2)
0 件の賞賛
返信
1 返信

1,438件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello parag,

 

1. The MX8X has the GPU7000Lite but not have NPU. the eIQ that can access is on L5.4.70.

2. The eIQ documents are in your yocto relases.

3. Is in the L5.4.70 BSP

4. you can download the demos from https://github.com/NXPmicro/gtec-demo-framework

 

Regards

 

0 件の賞賛
返信