LPDDR4 Capacity for IMX8M Mini

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPDDR4 Capacity for IMX8M Mini

ソリューションへジャンプ
9,715件の閲覧回数
haryanl
Contributor IV

Hello,

I'm planning to change 2GB LPDDR4 to 4GB for the IMX8M Mini Quad board.

Or change 2GB to 1/2/4 / 8GB
→Is there a problem, when not changing the hardware design?

Many Thanks.

1 解決策
9,075件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

The 4GB can work. And for 8GB DRAM, lower 3GB can be accessed by all the modules, higher 5GB is A53 CPU only.

Hope this can do help for you.

元の投稿で解決策を見る

13 返答(返信)
9,076件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

The 4GB can work. And for 8GB DRAM, lower 3GB can be accessed by all the modules, higher 5GB is A53 CPU only.

Hope this can do help for you.

8,793件の閲覧回数
NATHANKLOGIC
Contributor III

Hi

Is the higher 5GB available to any configuration of the A53 or only when using a Quad-A53?  The following note is in the i.MX 8M Mini RM that specifically states the "Quad-A53".  It is not clear to me why it would be the Quad configuration only.

NATHANKLOGIC_0-1616085320830.png

Thanks!

0 件の賞賛
返信
9,075件の閲覧回数
haryanl
Contributor IV

Hi Rita Wang,

(I decided to use 2GB LPDDR4)
But, Can you show me, can I use LPDDR4 500MB for mini IMX8M

I just want more information
Thank you very much

0 件の賞賛
返信
9,075件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

If you are using the 2GB LPDDR4, you can refer to our reference design.

0 件の賞賛
返信
9,075件の閲覧回数
haryanl
Contributor IV

yes, that's right, I did refer to the reference circuit.
But my superior wants to confirm the above information
Please confirm to me

Many Thanks

0 件の賞賛
返信
9,075件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Confirm "LPDDR4 500MB for mini IMX8M"? I am confused

9,075件の閲覧回数
haryanl
Contributor IV

yes, is it

0 件の賞賛
返信
9,074件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

If you do not use the GPU,VPU, the 512MB can work. But do not recommend you to use. You can use 2GB as our reference design.

0 件の賞賛
返信
9,075件の閲覧回数
haryanl
Contributor IV

Thanks for your support
I used 2GB LPDDR4 and it worked properly

0 件の賞賛
返信
9,074件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Good~~

0 件の賞賛
返信
9,074件の閲覧回数
haryanl
Contributor IV

Thank you for your support

0 件の賞賛
返信
9,075件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

I need to confirm it for you and then give you reply.

Have a nice day

Rita

0 件の賞賛
返信
9,075件の閲覧回数
haryanl
Contributor IV

Thank you
I would appreciate your favor

0 件の賞賛
返信