LCD display with 8080 interface is not normal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD display with 8080 interface is not normal

Jump to solution
2,180 Views
lvmh
Contributor I

Hi,all

I am debugging the LCD interface for 8080 series, but the display color is greenish, and the whole screen displays four

I am  working with kernel 4.1.15v,The CPU used for the board the company painted itself is imx6ul.

pictures. ps:Modified according to the patch:Patch to support MPU 8080 LCD on iMX6UL and iMX7D

Can someone give me some advice?Thanks!

0 Kudos
Reply
1 Solution
2,049 Views
joanxie
NXP TechSupport
NXP TechSupport

did you modify and test refer to the document as below? if yes, could you share the test log file? it seems the de-interlacing issue, check if you set the panel correct or not.

https://community.nxp.com/docs/DOC-331754?commentID=47960#comment-47960 

View solution in original post

0 Kudos
Reply
1 Reply
2,050 Views
joanxie
NXP TechSupport
NXP TechSupport

did you modify and test refer to the document as below? if yes, could you share the test log file? it seems the de-interlacing issue, check if you set the panel correct or not.

https://community.nxp.com/docs/DOC-331754?commentID=47960#comment-47960 

0 Kudos
Reply