LCD display with 8080 interface is not normal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LCD display with 8080 interface is not normal

跳至解决方案
3,058 次查看
lvmh
Contributor I

Hi,all

I am debugging the LCD interface for 8080 series, but the display color is greenish, and the whole screen displays four

I am  working with kernel 4.1.15v,The CPU used for the board the company painted itself is imx6ul.

pictures. ps:Modified according to the patch:Patch to support MPU 8080 LCD on iMX6UL and iMX7D

Can someone give me some advice?Thanks!

0 项奖励
回复
1 解答
2,927 次查看
joanxie
NXP TechSupport
NXP TechSupport

did you modify and test refer to the document as below? if yes, could you share the test log file? it seems the de-interlacing issue, check if you set the panel correct or not.

https://community.nxp.com/docs/DOC-331754?commentID=47960#comment-47960 

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,928 次查看
joanxie
NXP TechSupport
NXP TechSupport

did you modify and test refer to the document as below? if yes, could you share the test log file? it seems the de-interlacing issue, check if you set the panel correct or not.

https://community.nxp.com/docs/DOC-331754?commentID=47960#comment-47960 

0 项奖励
回复