LCD display with 8080 interface is not normal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCD display with 8080 interface is not normal

ソリューションへジャンプ
3,141件の閲覧回数
lvmh
Contributor I

Hi,all

I am debugging the LCD interface for 8080 series, but the display color is greenish, and the whole screen displays four

I am  working with kernel 4.1.15v,The CPU used for the board the company painted itself is imx6ul.

pictures. ps:Modified according to the patch:Patch to support MPU 8080 LCD on iMX6UL and iMX7D

Can someone give me some advice?Thanks!

0 件の賞賛
返信
1 解決策
3,010件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

did you modify and test refer to the document as below? if yes, could you share the test log file? it seems the de-interlacing issue, check if you set the panel correct or not.

https://community.nxp.com/docs/DOC-331754?commentID=47960#comment-47960 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,011件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

did you modify and test refer to the document as below? if yes, could you share the test log file? it seems the de-interlacing issue, check if you set the panel correct or not.

https://community.nxp.com/docs/DOC-331754?commentID=47960#comment-47960 

0 件の賞賛
返信