LCD INTERFACE WITH IMX6 SABRE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCD INTERFACE WITH IMX6 SABRE

ソリューションへジャンプ
3,565件の閲覧回数
venkat_c
Contributor I

Hi Everyone,

We are planning to use "BD070LIC1 – 7″ 1280×800 Display" with Touchscreen for our project.

The connectors in the LCD + Touchscreen is not compatible with our host board, So we have decided to use a intermediate connector board.

Details of the host board :

  • Freescale i.MX6 Sabre SDP
  • Android 5.0.1

Please find attached schematics, Can anyone please make sure the LCD will work with Sabre SDP. Also recommend if any other 7" LVDS LCD is compatible for our host board.

Ref:

Host board - SABRE for Smart Devices Reference Design|Freescale

Original present Working LCD - http://boundarydevices.com/wp-content/uploads/2013/06/HSD100PXN1-A00-C11-1.0.pdf

The LCD we are going to use - http://boundarydevices.com/wp-content/uploads/2014/12/HSD070PWW1-B01.pdf

The Touchscreen we are going to use - http://boundarydevices.com/wp-content/uploads/2015/05/SE-CTPGG7007.pdf#page=1&zoom=170,402,836

Regards,

Venkat

ラベル(5)
タグ(1)
0 件の賞賛
返信
1 解決策
3,119件の閲覧回数
art
NXP Employee
NXP Employee

The solution you consider seems to be the working one. You then have to adjust the screen resolution parameters in display driver and correctly handle the touchscreen by I2C interface.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,120件の閲覧回数
art
NXP Employee
NXP Employee

The solution you consider seems to be the working one. You then have to adjust the screen resolution parameters in display driver and correctly handle the touchscreen by I2C interface.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信