LCD INTERFACE WITH IMX6 SABRE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD INTERFACE WITH IMX6 SABRE

Jump to solution
3,547 Views
venkat_c
Contributor I

Hi Everyone,

We are planning to use "BD070LIC1 – 7″ 1280×800 Display" with Touchscreen for our project.

The connectors in the LCD + Touchscreen is not compatible with our host board, So we have decided to use a intermediate connector board.

Details of the host board :

  • Freescale i.MX6 Sabre SDP
  • Android 5.0.1

Please find attached schematics, Can anyone please make sure the LCD will work with Sabre SDP. Also recommend if any other 7" LVDS LCD is compatible for our host board.

Ref:

Host board - SABRE for Smart Devices Reference Design|Freescale

Original present Working LCD - http://boundarydevices.com/wp-content/uploads/2013/06/HSD100PXN1-A00-C11-1.0.pdf

The LCD we are going to use - http://boundarydevices.com/wp-content/uploads/2014/12/HSD070PWW1-B01.pdf

The Touchscreen we are going to use - http://boundarydevices.com/wp-content/uploads/2015/05/SE-CTPGG7007.pdf#page=1&zoom=170,402,836

Regards,

Venkat

Tags (1)
0 Kudos
Reply
1 Solution
3,101 Views
art
NXP Employee
NXP Employee

The solution you consider seems to be the working one. You then have to adjust the screen resolution parameters in display driver and correctly handle the touchscreen by I2C interface.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
3,102 Views
art
NXP Employee
NXP Employee

The solution you consider seems to be the working one. You then have to adjust the screen resolution parameters in display driver and correctly handle the touchscreen by I2C interface.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply