LCD Display contrast/gamma adjustment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCD Display contrast/gamma adjustment

ソリューションへジャンプ
2,168件の閲覧回数
slimSHA
Contributor III
We have a 7 inch LCD display connected to our SOC (IMX6) and a QTE-based application is running on it (No X Window system). 
Everything is fine but the LCD contrast is not that good. The colors need to be a little darker. 
we have tried adjusting gamma using MXCFB_SET_GAMMA ioctl (the source code is attached) and were able to see some changes in the color. but the colors are distorted. 
How to properly adjust the gamma/contrast of an LCD screen? 
 
any help is appreciated. 
Thanks in advance.
 
ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,164件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
1 返信
2,165件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Thejas

 

may be useful to look at unit test examples

https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_fb_test?h=lf-5.10.52_2.1.0

 

Best regards
igor