i.MX 6SoloX: EIM: Continuous BCLK in async Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6SoloX: EIM: Continuous BCLK in async Mode

Jump to solution
618 Views
Posch
Contributor I

Hi,

I'm working on a project, in which I want to use the EIM of an i.MX 6SoloX to connect to a FPGA. I want to use the EIM in async mode with continuous BCLK as a reference for the FPGA.

The appnote AN2680 says on page 12: "The burst clock (BCLK) follows the timing of the internal system clock (HCLK), in that the frequency of the system clock (HCLK) is mirrored on the external burst clock (BCLK) output.". This appnote not directly applies to the i.MX 6SoloX. Is the above mentioned statement also vaild for the i.MX 6SoloX? Can i use the EIM in async mode with continuous BCLK to access the FPGA in single word write/read operation?

Thanks, Robin

0 Kudos
Reply
1 Solution
615 Views
igorpadykov
NXP Employee
NXP Employee

Hi Robin

 

>Can i use the EIM in async mode with continuous BCLK..

 

not sorry. It is applicable only to synchronous mode, as described

in sect.23.5.1 Continuous BCLK    i.MX 6SoloX Applications Processor Reference Manual

1.jpg

Best regards
igor

 

View solution in original post

1 Reply
616 Views
igorpadykov
NXP Employee
NXP Employee

Hi Robin

 

>Can i use the EIM in async mode with continuous BCLK..

 

not sorry. It is applicable only to synchronous mode, as described

in sect.23.5.1 Continuous BCLK    i.MX 6SoloX Applications Processor Reference Manual

1.jpg

Best regards
igor