LCD Display contrast/gamma adjustment

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LCD Display contrast/gamma adjustment

跳至解决方案
2,167 次查看
slimSHA
Contributor III
We have a 7 inch LCD display connected to our SOC (IMX6) and a QTE-based application is running on it (No X Window system). 
Everything is fine but the LCD contrast is not that good. The colors need to be a little darker. 
we have tried adjusting gamma using MXCFB_SET_GAMMA ioctl (the source code is attached) and were able to see some changes in the color. but the colors are distorted. 
How to properly adjust the gamma/contrast of an LCD screen? 
 
any help is appreciated. 
Thanks in advance.
 
标签 (1)
标记 (3)
0 项奖励
回复
1 解答
2,163 次查看
igorpadykov
NXP Employee
NXP Employee
1 回复
2,164 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Thejas

 

may be useful to look at unit test examples

https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_fb_test?h=lf-5.10.52_2.1.0

 

Best regards
igor