When running GPU SDK examples (i.e. IMX6_GPU_SDK) using L3.0.35_4.1.0 on i.MX6Q, it often gives kernel panic. Here are some facts and observations:
Here are the typical debug outputs for the kernel panic:
fbdev version:
root@localhost:/gpu_sdk_v1.00/Samples/GLES2.0/bin/GLES20_fbdev# ./02_ColoredTriangle
Internal error: Oops - undefined instruction: 0 [#1] PREEMPT SMP
Modules linked in: vivante drm tw9912_tvin
CPU: 0 Not tainted (3.0.35-2666-gbdde708 #1)
PC is at rb_erase+0x40/0x36c
LR is at timerqueue_del+0x34/0x88
pc : [<8022de7c>] lr : [<8022f2d4>] psr: a0000093
sp : 806f3f28 ip : 00000000 fp : 00000000
r10: 8c0084b8 r9 : 00000000 r8 : 8c008568
r7 : 00000043 r6 : 00000000 r5 : 8c0084c4 r4 : 8c008568
r3 : ba38fad0 r2 : ba92db68 r1 : 8c0084c4 r0 : 8c008568
Flags: NzCv IRQs off FIQs on Mode SVC_32 ISA ARM Segment kernel
Control: 10c53c7d Table: 49a6404a DAC: 00000015
Process swapper (pid: 0, stack limit = 0x806f22f0)
Stack: (0x806f3f28 to 0x806f4000)
3f20: 8c008568 8c0084c4 00000000 8022f2d4 00000001 ba47fb58
3f40: 00000000 8008b5d4 8c008568 00000001 00000000 00000043 8c008568 412fc09a
3f60: 80707cc0 8008b934 04da0191 a0000093 8c008568 00000043 00000000 8008b954
3f80: 04da0191 80098010 8070ae7c 412fc09a 04da0191 00000043 00000000 806f2000
3fa0: 8074e244 80707a6c 80507b10 8070ae7c 00000000 8003dce4 80707b3c 8074e1a0
3fc0: 8002c7f0 8c005100 1000406a 80008868 800082f8 00000000 00000000 8002c7f0
3fe0: 00000000 10c53c7d 80707a8c 8002c7ec 8070ae74 10008040 00000000 00000000
[<8022de7c>] (rb_erase+0x40/0x36c) from [<8022f2d4>] (timerqueue_del+0x34/0x88)
[<8022f2d4>] (timerqueue_del+0x34/0x88) from [<8008b5d4>] (__remove_hrtimer+0x38/0xd0)
[<8008b5d4>] (__remove_hrtimer+0x38/0xd0) from [<8008b934>] (hrtimer_try_to_cancel+0x8c/0x98)
[<8008b934>] (hrtimer_try_to_cancel+0x8c/0x98) from [<8008b954>] (hrtimer_cancel+0x14/0x20)
[<8008b954>] (hrtimer_cancel+0x14/0x20) from [<80098010>] (tick_nohz_restart_sched_tick+0x128/0x1ec)
[<80098010>] (tick_nohz_restart_sched_tick+0x128/0x1ec) from [<8003dce4>] (cpu_idle+0xa4/0x124)
[<8003dce4>] (cpu_idle+0xa4/0x124) from [<80008868>] (start_kernel+0x248/0x288)
[<80008868>] (start_kernel+0x248/0x288) from [<10008040>] (0x10008040)
Code: 1afffffb e5902000 e3d22003 05853000 (1a000049)
X11 version:
root@localhost:/gpu_sdk_v1.00/Samples/GLES1.1/bin/GLES11_x11# ./01_SimpleTriangle
Lesson 02
chooseconfig,
createwindow,
creatcontext,
makecurrent,
exiting init,
Unable to handle kernel paging request at virtual address a8689105
pgd = ba0f8000
[a8689105] *pgd=00000000
Internal error: Oops: 805 [#1] PREEMPT SMP
Modules linked in: mxc_v4l2_capture ipu_fg_overlay_sdc ipu_csi_enc ipu_prp_enc ipu_still ipu_bg_overlay_sdc vivante drm g_ncm pn544_i2c pn544 tw9912_tvin
CPU: 0 Not tainted (3.0.35-2666-gbdde708 #1)
PC is at timerqueue_add+0x54/0xc4
LR is at 0xffffffff
pc : [<8022f37c>] lr : [<ffffffff>] psr: 600f0093
sp : 806f3ef8 ip : 00000000 fp : 00000000
r10: 8c0084b8 r9 : 80035480 r8 : 8c008568
r7 : 00000038 r6 : 8c0084c4 r5 : 8c008568 r4 : 8074ec10
r3 : 8074ec08 r2 : bcac8e00 r1 : 0000000d r0 : a8689100
Flags: nZCv IRQs off FIQs on Mode SVC_32 ISA ARM Segment kernel
Control: 10c53c7d Table: 4a0f804a DAC: 00000015
Process swapper (pid: 0, stack limit = 0x806f22f0)
Stack: (0x806f3ef8 to 0x806f4000)
3ee0: 0000000d 8c008568
3f00: 8c0084b8 8c0084b8 00000038 8008b2fc 0000000d a8689100 00000000 8008bd1c
3f20: a8689100 0000000d 806f2000 80707cc0 80035480 00000000 a999be00 00000000
3f40: 00000000 a00f0093 8c008568 a8689100 0000000d 00000000 00000000 8c008568
3f60: 412fc09a 80755638 00000000 8008c01c 00000000 00000002 00000001 80755638
3f80: 00000000 800980a4 00000000 00000002 a7e22485 0000000d 00000000 806f2000
3fa0: 8074e244 80707a6c 80507b10 8070ae7c 00000000 8003dce4 80707b3c 8074e1a0
3fc0: 8002c7f0 8c005100 1000406a 80008868 800082f8 00000000 00000000 8002c7f0
3fe0: 00000000 10c53c7d 80707a8c 8002c7ec 8070ae74 10008040 00000000 00000000
[<8022f37c>] (timerqueue_add+0x54/0xc4) from [<8008b2fc>] (enqueue_hrtimer+0x18/0x50)
[<8008b2fc>] (enqueue_hrtimer+0x18/0x50) from [<8008bd1c>] (__hrtimer_start_range_ns+0x134/0x3e4)
[<8008bd1c>] (__hrtimer_start_range_ns+0x134/0x3e4) from [<8008c01c>] (hrtimer_start_range_ns+0x24/0x2c)
[<8008c01c>] (hrtimer_start_range_ns+0x24/0x2c) from [<800980a4>] (tick_nohz_restart_sched_tick+0x1bc/0x1ec)
[<800980a4>] (tick_nohz_restart_sched_tick+0x1bc/0x1ec) from [<8003dce4>] (cpu_idle+0xa4/0x124)
[<8003dce4>] (cpu_idle+0xa4/0x124) from [<80008868>] (start_kernel+0x248/0x288)
[<80008868>] (start_kernel+0x248/0x288) from [<10008040>] (0x10008040)
Code: e594c000 e35c0000 1afffff5 e5853000 (e1a00005)
---[ end trace d5ce71d1d3963135 ]---
Kernel panic - not syncing: Attempted to kill the idle task!
[<80043854>] (unwind_backtrace+0x0/0xf8) from [<804ff734>] (panic+0x74/0x18c)
[<804ff734>] (panic+0x74/0x18c) from [<80071b58>] (do_exit+0x684/0x6e8)
[<80071b58>] (do_exit+0x684/0x6e8) from [<80040740>] (die+0x228/0x284)
[<80040740>] (die+0x228/0x284) from [<804ff52c>] (__do_kernel_fault.part.4+0x54/0x74)
[<804ff52c>] (__do_kernel_fault.part.4+0x54/0x74) from [<80047570>] (do_translation_fault+0x0/0xa0)
[<80047570>] (do_translation_fault+0x0/0xa0) from [<00000000>] ( (null))
CPU3: stopping
[<80043854>] (unwind_backtrace+0x0/0xf8) from [<80037324>] (do_IPI+0x150/0x17c)
[<80037324>] (do_IPI+0x150/0x17c) from [<8003ca0c>] (__irq_svc+0x4c/0xe8)
Exception stack(0xbff01ef0 to 0xbff01f38)
1ee0: bff01f38 0000000a 00000000 00000003
1f00: 00000082 bff00000 bff00000 00000000 80753cc0 00000003 806f4040 00000000
1f20: 80043154 bff01f38 80073f34 80073998 20000113 ffffffff
[<8003ca0c>] (__irq_svc+0x4c/0xe8) from [<80073998>] (__do_softirq+0x4c/0x140)
[<80073998>] (__do_softirq+0x4c/0x140) from [<80073f34>] (irq_exit+0x94/0x9c)
[<80073f34>] (irq_exit+0x94/0x9c) from [<800372e0>] (do_IPI+0x10c/0x17c)
[<800372e0>] (do_IPI+0x10c/0x17c) from [<8003ca0c>] (__irq_svc+0x4c/0xe8)
Exception stack(0xbff01f90 to 0xbff01fd8)
1f80: 80755620 80000093 00000001 00000000
1fa0: bff00000 8074e244 80707a6c 80507b10 8070ae7c 412fc09a 00000000 00000000
1fc0: 00000000 bff01fd8 8004b76c 8003db04 40000013 ffffffff
[<8003ca0c>] (__irq_svc+0x4c/0xe8) from [<8003db04>] (default_idle+0x24/0x28)
[<8003db04>] (default_idle+0x24/0x28) from [<8003dd20>] (cpu_idle+0xe0/0x124)
[<8003dd20>] (cpu_idle+0xe0/0x124) from [<104fc574>] (0x104fc574)
CPU1: stopping
[<80043854>] (unwind_backtrace+0x0/0xf8) from [<80037324>] (do_IPI+0x150/0x17c)
[<80037324>] (do_IPI+0x150/0x17c) from [<8003ca0c>] (__irq_svc+0x4c/0xe8)
Exception stack(0xbffadf90 to 0xbffadfd8)
df80: 80755620 80070093 00000001 00000000
dfa0: bffac000 8074e244 80707a6c 80507b10 8070ae7c 412fc09a 00000000 00000000
dfc0: 00000000 bffadfd8 8004b76c 8003db04 40070013 ffffffff
[<8003ca0c>] (__irq_svc+0x4c/0xe8) from [<8003db04>] (default_idle+0x24/0x28)
[<8003db04>] (default_idle+0x24/0x28) from [<8003dd20>] (cpu_idle+0xe0/0x124)
[<8003dd20>] (cpu_idle+0xe0/0x124) from [<104fc574>] (0x104fc574)
CPU2: stopping
[<80043854>] (unwind_backtrace+0x0/0xf8) from [<80037324>] (do_IPI+0x150/0x17c)
[<80037324>] (do_IPI+0x150/0x17c) from [<8003ca0c>] (__irq_svc+0x4c/0xe8)
Exception stack(0xbffb5f90 to 0xbffb5fd8)
5f80: 80755620 60070093 00000001 00000000
5fa0: bffb4000 8074e244 80707a6c 80507b10 8070ae7c 412fc09a 00000000 00000000
5fc0: 00000000 bffb5fd8 8004b76c 8003db04 40070013 ffffffff
[<8003ca0c>] (__irq_svc+0x4c/0xe8) from [<8003db04>] (default_idle+0x24/0x28)
[<8003db04>] (default_idle+0x24/0x28) from [<8003dd20>] (cpu_idle+0xe0/0x124)
[<8003dd20>] (cpu_idle+0xe0/0x124) from [<104fc574>] (0x104fc574)
Is there any hint from the debug output above, or any suggestion to debug the problem on our board? Please advise.
 
					
				
		
 andre_silva
		
			andre_silva
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		I just got the GPU SDK package from FSL website and tested on the latest BSP release, also got from the FSL website, everything worked fine with no issues nor crashes.
 
					
				
		
 karina_valencia
		
			karina_valencia
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		AndreSilva Oct 15, 2013 6:08 AM (in response to Dan Wang)
Did yo get the GPU libraries you used on ubuntu from Ltib package ?