i.mx53 SATA link down (SStatus 0 SControl 300)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx53 SATA link down (SStatus 0 SControl 300)

ソリューションへジャンプ
5,708件の閲覧回数
davee
Contributor III

Hi all,

linux 2.6.35.3

i.mx53

kingston SSD 128GB sata

I've got a i.mx53 board based on the imx53qsb and i'm trying to use the SATA connection during boot up I see:

scsi0 : ahci

ata1: SATA max UDMA/133 mmio [mem 0x10000000-0x10000fff] port 0x100 irq 28

then not long later it comes up with:

ata1: SATA link down (SStatus 0 SControl 300)

I've tried sending "0 0 0" to /sys/class/scsi_host/host0/scan

which resulted in

ata1: hard resetting link

ata1: SATA link down (SStatus 0 SControl 300)

ata1: EH complete

Can someone aid me in tracking the problem down, the Google search results don't seems to resolve to anything?

Regards

Dave

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
4,684件の閲覧回数
davee
Contributor III

In reply to myself I swapped out the SSD and the new drive although a 1.5GHz than the original 3GHz sata works apparently correctly, so the drive had gone bad.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
4,685件の閲覧回数
davee
Contributor III

In reply to myself I swapped out the SSD and the new drive although a 1.5GHz than the original 3GHz sata works apparently correctly, so the drive had gone bad.

0 件の賞賛
返信