JTAG debugger i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JTAG debugger i.MX6

3,557 Views
vignan
Contributor I

What JTAG debugger is recommended for i.MX6?

Tags (2)
0 Kudos
Reply
4 Replies

2,407 Views
MikeJones
Contributor III

My PEEDI works well. Presents all cores as a single core so that GDB can debug an SMP application. I have config files at ecosfreescale.sourceforge.com in the files area.

0 Kudos
Reply

2,407 Views
sinanakman
Senior Contributor III

We regularly use BDI3000 from Abatron.

Regards

Sinan Akman

0 Kudos
Reply

2,407 Views
LeonardoSandova
Specialist I

ARM DSTREAM is also a good option.

0 Kudos
Reply

2,407 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Vignan,

We use the RealView debugger with the RealView ICE and it works great.

Best regards.

Jorge.

0 Kudos
Reply