JTAG debugger i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JTAG debugger i.MX6

3,561件の閲覧回数
vignan
Contributor I

What JTAG debugger is recommended for i.MX6?

タグ(2)
0 件の賞賛
返信
4 返答(返信)

2,411件の閲覧回数
MikeJones
Contributor III

My PEEDI works well. Presents all cores as a single core so that GDB can debug an SMP application. I have config files at ecosfreescale.sourceforge.com in the files area.

0 件の賞賛
返信

2,411件の閲覧回数
sinanakman
Senior Contributor III

We regularly use BDI3000 from Abatron.

Regards

Sinan Akman

0 件の賞賛
返信

2,411件の閲覧回数
LeonardoSandova
Specialist I

ARM DSTREAM is also a good option.

0 件の賞賛
返信

2,411件の閲覧回数
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Vignan,

We use the RealView debugger with the RealView ICE and it works great.

Best regards.

Jorge.

0 件の賞賛
返信