Issues with iMX8ULP BSDL Files

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issues with iMX8ULP BSDL Files

2,853 次查看
kharding
Contributor I

Hi,

I have been following AN13215 to perform a boundary-scan proof-of-concept with the specified Lauterbach devices/sw, but have a few issues.

I downloaded the iMX8ULP BSDL files, but noticed that the two files are switched. We are using the 15x15 package which supposedly corresponds to the IMX8ULP-BSDL.zip file, but the file that matches it(and the GPIOs) is actually in MCIMX8ULP-EVK9-BSDL.zip:

kharding_1-1739895359129.png

It makes sense that we want the EVK file as the 15x15 is on the EVK.

I then proceed with the correct file, following the steps in the application note, and get stuck when the IDCODE is incorrect:

kharding_0-1739895277891.png

I was however able to successfully SAMPLEall and BYPASSall:

kharding_2-1739895619250.png

Can the files be corrected and can we have a file with the correct IDCODE?

Please don't hesitate to ask if you need more details.

Thank you for your support!

 

 

标签 (1)
0 项奖励
回复
7 回复数

2,828 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

he IDCODE for the DAP and boundary scan are different. If you have the JTAG_MOD properly set for debug mode and if you issue an IDCODE instruction you will receive the IDCODE for DAP. The one mentioned in the BSDL file is probably for the test mode.

Regards

0 项奖励
回复

2,697 次查看
Dennis_Griffith
Contributor I

Hello,

What are the values of the IDCODEs for DAP vs Boundary Scan mode?

0 项奖励
回复

2,824 次查看
kharding
Contributor I

Hi, @Bio_TICFSL ,

We are using the iMX8ULP and there is no JTAG_MOD or TEST_MODE GPIO. Is there another way to change it?

Best Regards,

kharding

0 项奖励
回复

2,801 次查看
kharding
Contributor I

Hi @Bio_TICFSL ,

It has been a few days and the issue remains unresolved. 

Your continued support would be greatly appreciated!

 

Best Regards,

kharding

0 项奖励
回复

2,778 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Sorry, but there is no way to changing.

Regards

0 项奖励
回复

2,765 次查看
kharding
Contributor I

Hi @Bio_TICFSL ,

 

Is there a way to change the IDCODE on an iMX8ULP(the iMX8ULP does not have TEST_MODE or JTAG_MOD GPIOs) to boundary scan?

 

Best Regards,

kharding

0 项奖励
回复

2,749 次查看
kharding
Contributor I

Hi @Bio_TICFSL ,

 

The IDCODE is the BSDL had the incorrect version. I changed it from "0000" to "0001" and now it now passes the IDCODE check.

 

Best regards,

kharding

0 项奖励
回复