Issue with mfgtool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue with mfgtool

6,563件の閲覧回数
victorien
Contributor IV

Hi,

I developed a board with an iMX28 processor and for mass production I need mfgtool to program the memory. Because it's for a custom board, I generate a new updater_ivt.sb

When I plug the board to the computer, mfgtool see the device.

When I press start, the firmware is download to the board and on the console, I see the boot log :

Linux version 2.6.35.3-g6475bb9-dirty (victorien@BENNEVIS) (gcc version 4.3.3 (4

CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177                  

CPU: VIVT data cache, VIVT instruction cache                                   

Machine: Ophrys Systemes Misu board rev002                                     

Memory policy: ECC disabled, Data cache writeback                              

On node 0 totalpages: 16384                                                    

free_area_init_node: node 0, pgdat c0324af0, node_mem_map c036b000             

  DMA zone: 32 pages used for memmap                                           

  DMA zone: 0 pages reserved                                                   

  DMA zone: 4064 pages, LIFO batch:0                                           

  Normal zone: 96 pages used for memmap                                        

  Normal zone: 12192 pages, LIFO batch:1                                       

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 16256     

Kernel command line: console=ttyAM0,115200                                     

PID hash table entries: 256 (order: -2, 1024 bytes)                            

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)                  

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)                   

Memory: 64MB = 64MB total                                                      

Memory: 57376k/57376k available, 8160k reserved, 0K highmem                    

Virtual kernel memory layout:                                                  

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)                              

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)                              

    DMA     : 0xfde00000 - 0xffe00000   (  32 MB)                              

    vmalloc : 0xc4800000 - 0xf0000000   ( 696 MB)                              

    lowmem  : 0xc0000000 - 0xc4000000   (  64 MB)                              

    modules : 0xbf000000 - 0xc0000000   (  16 MB)                              

      .init : 0xc0008000 - 0xc0027000   ( 124 kB)                              

      .text : 0xc0027000 - 0xc0305000   (2936 kB)                              

      .data : 0xc0306000 - 0xc03254e0   ( 126 kB)                              

SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1        

Hierarchical RCU implementation.                                               

        RCU-based detection of stalled CPUs is disabled.                       

        Verbose stalled-CPUs detection is disabled.                            

NR_IRQS:288                                                                    

Console: colour dummy device 80x30                                             

console [ttyAM0] enabled                                                       

Calibrating delay loop... 226.09 BogoMIPS (lpj=1130496)                        

pid_max: default: 32768 minimum: 301                                           

Mount-cache hash table entries: 512                                            

CPU: Testing write buffer coherency: ok                                        

regulator: core version 0.5                                                    

NET: Registered protocol family 16                                             

regulator: vddd: 800 <--> 1575 mV at 1500 mV fast normal                       

regulator: vdddbo: 800 <--> 1575 mV fast normal                                

regulator: vdda: 1500 <--> 2275 mV at 1800 mV fast normal                      

vddio = 3380000, val=10                                                        

regulator: vddio: 2880 <--> 3680 mV at 3380 mV fast normal                     

regulator: overall_current: fast normal                                        

regulator: vbus5v:                                                             

regulator: mxs-duart-1: fast normal                                            

regulator: mxs-bl-1: fast normal                                               

regulator: mxs-i2c-1: fast normal                                              

regulator: mmc_ssp-1: fast normal                                              

regulator: mmc_ssp-2: fast normal                                              

regulator: charger-1: fast normal                                              

regulator: power-test-1: fast normal                                           

regulator: cpufreq-1: fast normal                                              

i.MX IRAM pool: 124 KB@0xc4820000                                              

usb DR wakeup device is registered                                             

IMX usb wakeup probe                                                           

the wakeup pdata is 0xc030e514                                                 

audit: cannot initialize inotify handle                                        

bio: create slab <bio-0> at 0                                                  

SCSI subsystem initialized                                                     

Switching to clocksource mxs clock source                                      

Trying to unpack rootfs image as initramfs...                                  

Freeing initrd memory: 4096K                                                   

Bus freq driver module loaded                                                  

mxs_cpu_init: cpufreq init finished                                            

audit: initializing netlink socket (disabled)                                  

type=2000 audit(1.340:1): initialized                                          

JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.                            

msgmni has been set to 120                                                     

Block layer SCSI generic (bsg) driver version 0.4 loaded (major 253)           

io scheduler noop registered (default)                                         

Console: switching to colour frame buffer device 100x30                        

mxs-duart.0: ttyAM0 at MMIO 0x80074000 (irq = 47) is a DebugUART               

mxs-auart.0: ttySP0 at MMIO 0x8006a000 (irq = 112) is a mxs-auart.0            

Found APPUART 3.1.0                                                            

mxs-auart.1: ttySP1 at MMIO 0x8006c000 (irq = 113) is a mxs-auart.1            

Found APPUART 3.1.0                                                            

mxs-auart.2: ttySP2 at MMIO 0x8006e000 (irq = 114) is a mxs-auart.2            

Found APPUART 3.1.0                                                            

mxs-auart.3: ttySP3 at MMIO 0x80070000 (irq = 115) is a mxs-auart.3            

Found APPUART 3.1.0                                                            

mxs-auart.4: ttySP4 at MMIO 0x80072000 (irq = 116) is a mxs-auart.4            

Found APPUART 3.1.0                                                            

brd: module loaded                                                             

loop: module loaded                                                            

Loading iSCSI transport class v2.0-870.                                        

i.MX GPMI NFC                                                                  

NFC: Version 1, 8-chip GPMI and BCH                                            

gpmi-nfc: probe of gpmi-nfc.0 failed with error 1                              

ARC USBOTG Device Controller driver (1 August 2005)                            

check_parameters:UTP settings are in place now, overriding defaults            

g_file_storage gadget: File-backed Storage Gadget, version: 20 November 2008   

g_file_storage gadget: Number of LUNs=1                                        

dr_controller_run: udc out low power mode                                      

fsl-usb2-udc: bind to driver g_file_storage                                    

mice: PS/2 mouse device common for all mice                                    

input: mxs-kbd as /devices/platform/mxs-kbd.0/input/input0                     

input: MXS touchscreen as /devices/virtual/input/input1                        

MXS RTC driver v1.0 hardware v2.3.0                                            

mxs-rtc mxs-rtc.0: rtc core: registered mxs-rtc as rtc0                        

mxs-mmc: MXS SSP Controller MMC Interface driver                               

mxs-mmc mxs-mmc.0: mmc0: MXS SSP MMC DMAIRQ 82 ERRIRQ 96                       

Registered led device: led1:red                                                

Registered led device: led2:green                                              

mxs-rtc mxs-rtc.0: setting system clock to 1970-01-01 00:00:33 UTC (33)        

Freeing init memory: 124K                                                      

mmc0: new high speed SDHC card at address 0002                                 

mmcblk0: mmc0:0002 00000 7.41 GiB                                              

mmcblk0: p1                                                                   

charger------ ddi_bc_gBrokenReason=4

and at the and, the kernel launch usb gadget module :

root@freescale /$ g_file_storage gadget: high speed config #1

At this moment, it seem correct. but when mfgtool execute the first push command, I have this message on mfgtool

Operation is not completed.,failed to run command: type="push" body="mknod block,mmcblk0,/dev/mmcblk0,block" file="" timeout="" onERROR="" text=""

and this message on board console

Unable to handle kernel NULL pointer dereference at virtual address 00000009   

pgd = c0004000                                                                 

[00000009] *pgd=00000000                                                       

Internal error: Oops: 17 [#1]                                                  

last sysfs file:                                                               

CPU: 0    Not tainted  (2.6.35.3-g6475bb9-dirty #1051)                         

PC is at do_scsi_command+0x5bc/0x1aa8                                          

LR is at do_scsi_command+0x5bc/0x1aa8                                          

pc : [<c0222850>]    lr : [<c0222850>]    psr: 60000013                        

sp : c2c05e88  ip : c2c05e88  fp : c2c05f04                                    

r10: c03692ac  r9 : c3c32e00  r8 : 0000c036                                    

r7 : 00c03692  r6 : 00000000  r5 : c2c088a0  r4 : c03692d0                     

r3 : c03692d0  r2 : 00000001  r1 : 00000000  r0 : c03692bc                     

Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment kernel            

Control: 0005317f  Table: 42c7c000  DAC: 00000017                              

Process file-storage-ga (pid: 885, stack limit = 0xc2c04270)                   

Stack: (0xc2c05e88 to 0xc2c06000)                                              

5e80:                   c2c05eac c2c05e98 c2c2e000 c0309d70 c2c05ec4 c2c05ea8  

5ea0: 000000c0 c3c32e78 00000000 c2c184c0 c03692bc c2c2e000 c2c05eec 00000000  

5ec0: c2c088a0 c0055b0c c2c05ec8 c2c05ec8 00000200 c3c32e78 c3c32e40 c339c000  

5ee0: c3c32e00 00000200 c3c32e78 c3c32e40 c3c32e58 c2c04000 c2c05fc4 c2c05f08  

5f00: c02243c8 c02222a4 c3c32e7c c2c05f18 c003d344 c3c32eb0 0000000a 00000000  

5f20: 00000000 00000000 00000000 c0310028 c3c20038 c0310058 c3c20030 c0310058  

5f40: c2c05f64 c2c05f50 c3c2201c c2c088a0 00000017 c0318474 c2c04000 00000000  

5f60: c2c05f84 c2c05f70 c0318474 c3c20000 c2c05f9c c2c05f80 c003df70 c0070270  

5f80: 00000000 c2c088a0 c3c20000 c0318474 c2c05fc4 c2c05fa0 c027a904 c2c05fcc  

5fa0: c3c23ed0 c3c32e00 c0223d3c 00000000 00000000 00000000 c2c05ff4 c2c05fc8  

5fc0: c00556d8 c0223d4c 00000000 00000000 c2c05fd0 c2c05fd0 c3c23ed0 c0055650  

5fe0: c0044420 00000013 00000000 c2c05ff8 c0044420 c0055660 00000000 00000000  

Backtrace:                                                                     

[<c0222294>] (do_scsi_command+0x0/0x1aa8) from [<c02243c8>] (fsg_main_thread+0x)

[<c0223d3c>] (fsg_main_thread+0x0/0xa24) from [<c00556d8>] (kthread+0x88/0x90) 

[<c0055650>] (kthread+0x0/0x90) from [<c0044420>] (do_exit+0x0/0x5e8)          

r7:00000013 r6:c0044420 r5:c0055650 r4:c3c23ed0                               

Code: 11a06003 03a06000 e51b0054 eb0161cd (e5d62009)                           

---[ end trace c4cc3e0f4feb6a88 ]---   

I suppose ot miss something in ramrootfs or in kernel but I can't find what. Is there someone who have an idea ?

Best regards

ラベル(1)
0 件の賞賛
返信
12 返答(返信)

5,869件の閲覧回数
victorien
Contributor IV

Now I can generate updater_ivt.sb with ltib and it works on my board with mfgtools.

The download and programming work few time. But now the process always fails after the boot and the board is seeing as "Linux file storage gadget USB device" on mfgtools.

How resolve this problem ?

0 件の賞賛
返信

5,869件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi victorien

please create new Community thread.

~igor

0 件の賞賛
返信

5,869件の閲覧回数
victorien
Contributor IV

I installed ltib on a virtual machine with ubuntu 12.04 (I don't find how to do with newer version) and now I can compile with ltib.

I genrerate initramfs and use it on my usual toolchain to generate updater_ivt.sb (with my own zImage and bootlet). Unfortunately, It doesn't work and I have this log when I execute mfgtool :

0x8020a01d                                                                

HTLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLC

PowerPrep start initialize power...                                       
Battery Voltage = 1.86V                                                   
No valid battery detected. Power supply on 5V only                        
LLLLCOct 30 201415:55:01                                                  
FRAC 0x92925552                                                           
memory type is DDR2                                                       
               Wait for ddr ready 1 - 1130                            
power 0x00820616                                                          
Frac 0x92925552                                                           
start change cpu freq                                                     
hbus 0x00000003                                                           
cpu 0x00010001                                                            
start test external memory access                                         
ddr2 0x40000000                                                           
finish simple test                                                        
LLLLLLLFLCLFLLJUncompressing Linux... done, booting the kernel.           

Linux version 2.6.35.3-g6475bb9-dirty (victorien@BENNEVIS) (gcc version 4.3.3 (4

CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177             
CPU: VIVT data cache, VIVT instruction cache                              
Machine: Ophrys Systemes Misu board rev002                                
Memory policy: ECC disabled, Data cache writeback                         
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 16256
Kernel command line: console=ttyAM0,115200                                
PID hash table entries: 256 (order: -2, 1024 bytes)                       
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)             
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)              
Memory: 64MB = 64MB total                                                 
Memory: 55328k/55328k available, 10208k reserved, 0K highmem              
Virtual kernel memory layout:                                             
vector  : 0xffff0000 - 0xffff1000   (   4 kB)                         
fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)                         
DMA : 0xfde00000 - 0xffe00000   (  32 MB)                         
vmalloc : 0xc4800000 - 0xf0000000   ( 696 MB)                         
lowmem  : 0xc0000000 - 0xc4000000   (  64 MB)                         
modules : 0xbf000000 - 0xc0000000   (  16 MB)                         
  .init : 0xc0008000 - 0xc0027000   ( 124 kB)                         
  .text : 0xc0027000 - 0xc0305000   (2936 kB)                         
  .data : 0xc0306000 - 0xc0325580   ( 126 kB)                         
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1   
Hierarchical RCU implementation.                                          
    RCU-based detection of stalled CPUs is disabled.                  
    Verbose stalled-CPUs detection is disabled.                       
NR_IRQS:288                                                               
Console: colour dummy device 80x30                                        
console [ttyAM0] enabled                                                  
Calibrating delay loop... 226.09 BogoMIPS (lpj=1130496)                   
pid_max: default: 32768 minimum: 301                                      
Mount-cache hash table entries: 512                                       
CPU: Testing write buffer coherency: ok                                   
regulator: core version 0.5                                               
NET: Registered protocol family 16                                        
regulator: vddd: 800 <--> 1575 mV at 1500 mV fast normal                  
regulator: vdddbo: 800 <--> 1575 mV fast normal                           
regulator: vdda: 1500 <--> 2275 mV at 1800 mV fast normal                 
vddio = 3380000, val=10                                                   
regulator: vddio: 2880 <--> 3680 mV at 3380 mV fast normal                
regulator: overall_current: fast normal                                   
regulator: vbus5v:                                                        
regulator: mxs-duart-1: fast normal                                       
regulator: mxs-bl-1: fast normal                                          
regulator: mxs-i2c-1: fast normal                                         
regulator: mmc_ssp-1: fast normal                                         
regulator: mmc_ssp-2: fast normal                                         
regulator: charger-1: fast normal                                         
regulator: power-test-1: fast normal                                      
regulator: cpufreq-1: fast normal                                         
i.MX IRAM pool: 124 KB@0xc4820000                                         
usb DR wakeup device is registered                                        
IMX usb wakeup probe                                                      
audit: cannot initialize inotify handle                                   
bio: create slab <bio-0> at 0                                             
SCSI subsystem initialized                                                
Switching to clocksource mxs clock source                                 
Trying to unpack rootfs image as initramfs...                             
Freeing initrd memory: 6144K                                              
Bus freq driver module loaded                                             
mxs_cpu_init: cpufreq init finished                                       
audit: initializing netlink socket (disabled)                             
type=2000 audit(2.170:1): initialized                                     
JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.                      
msgmni has been set to 120                                                
Block layer SCSI generic (bsg) driver version 0.4 loaded (major 253)      
io scheduler noop registered (default)                                    
Console: switching to colour frame buffer device 100x30                   
mxs-duart.0: ttyAM0 at MMIO 0x80074000 (irq = 47) is a DebugUART          
mxs-auart.0: ttySP0 at MMIO 0x8006a000 (irq = 112) is a mxs-auart.0       
Found APPUART 3.1.0                                                       
mxs-auart.1: ttySP1 at MMIO 0x8006c000 (irq = 113) is a mxs-auart.1       
Found APPUART 3.1.0                                                       
mxs-auart.2: ttySP2 at MMIO 0x8006e000 (irq = 114) is a mxs-auart.2       
Found APPUART 3.1.0                                                       
mxs-auart.3: ttySP3 at MMIO 0x80070000 (irq = 115) is a mxs-auart.3       
Found APPUART 3.1.0                                                       
mxs-auart.4: ttySP4 at MMIO 0x80072000 (irq = 116) is a mxs-auart.4       
Found APPUART 3.1.0                                                       
brd: module loaded                                                        
loop: module loaded                                                       
Loading iSCSI transport class v2.0-870.                                   
i.MX GPMI NFC                                                             
NFC: Version 1, 8-chip GPMI and BCH                                       
gpmi-nfc: probe of gpmi-nfc.0 failed with error 1                         
ARC USBOTG Device Controller driver (1 August 2005)                       
check_parameters:UTP settings are in place now, overriding defaults       

g_file_storage gadget: File-backed Storage Gadget, version: 20 November 2008   

g_file_storage gadget: Number of LUNs=1                                   
fsl-usb2-udc: bind to driver g_file_storage                               
mice: PS/2 mouse device common for all mice                               
input: matrix-keypad as /devices/platform/matrix-keypad/input/input0      
input: MXS touchscreen as /devices/virtual/input/input1                   
MXS RTC driver v1.0 hardware v2.3.0                                       
mxs-rtc mxs-rtc.0: rtc core: registered mxs-rtc as rtc0                   
mxs-mmc: MXS SSP Controller MMC Interface driver                          
mxs-mmc mxs-mmc.0: mmc0: MXS SSP MMC DMAIRQ 82 ERRIRQ 96                  
mmc0: new high speed SDHC card at address 0002                            
charger------ ddi_bc_gBrokenReason=4                                      
mxs-rtc mxs-rtc.0: setting system clock to 1970-01-01 00:02:34 UTC (154)  
Freeing init memory: 124K                                                 
mmcblk0: mmc0:0002 00000 7.41 GiB                                         
starting pid 1694, tty '': '/etc/rc.d/rcS'                                
p1                                                                       
Mounting /proc and /sys                                                   
mount: wrong fs type, bad option, bad superblock on tmpfs,                
   missing codepage or helper program, or other error                 
   In some cases useful info is found in syslog - try                 
   dmesg | tail  or so                                                
                                                                          
mknod: /dev/console: File exists                                          
mknod: /dev/null: File exists                                             
Starting the hotplug events dispatcher udevd                              

udevd[1713]: init_udevd_socket: error getting socket: Address family not supporl

error initializing udevd socket                                           
udevd[1713]: main: error initializing udevd socket                        
Synthesizing initial hotplug events                                       
g_file_storage gadget: high speed config #1                               
Setting the hostname to freescale                                         
Mounting filesystems                                                      
mount: wrong fs type, bad option, bad superblock on shm,                  
   missing codepage or helper program, or other error                 
   In some cases useful info is found in syslog - try                 
   dmesg | tail  or so                                                
                                                                          
mount: wrong fs type, bad option, bad superblock on rwfs,                 
   missing codepage or helper program, or other error                 
   In some cases useful info is found in syslog - try                 
   dmesg | tail  or so                                                
                                                                          
mount: sysfs already mounted or /sys busy                                 
mount: according to mtab, /sys is already mounted on /sys                 
mount: mount point /proc/bus/usb does not exist                           
starting pid 1740, tty '': '/etc/rc.d/rc_gpu.S'                           
can't run '/etc/rc.d/rc_gpu.S': No such file or directory                 
starting pid 1741, tty '': '/sbin/getty -L ttyAM0 115200 vt100'           

process '/sbin/getty -L ttyAM0 115200 vt100' (pid 1741) exited. Scheduling for .

starting pid 1742, tty '': '/sbin/getty -L ttyAM0 115200 vt100'           

process '/sbin/getty -L ttyAM0 115200 vt100' (pid 1742) exited. Scheduling for .

starting pid 1743, tty '': '/sbin/getty -L ttyAM0 115200 vt100'           

I compile linux zImage with the same config as ltib but I think it's not enough. How can I create my custom board on ltib ?

0 件の賞賛
返信

5,869件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Please check documents below talking about some common issues met when

using i.mx28. Hope this will be useful for you.

Application note sharing: Issues often met in i.MX28 application

http://www.docin.com/touch_new/preview_new.do?id=735290638

0 件の賞賛
返信

5,869件の閲覧回数
victorien
Contributor IV

Thanks but I don't find any information to resolve my problem.

In my previous test, I just generate initramfs with ltib and I think it's necessary to generate the bootloader and the kernel with ltib. Unfortunatly, I don't find how to define a custom board on ltib. Is there a procedure to do that ?

0 件の賞賛
返信

5,869件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

I do not think that such kind of document is available,

in ltib you can select drivers which are used on your board and

change bootlets. I would suggest to look below

http://www.jann.cc/2013/08/31/porting_linux_to_a_new_board.html

0 件の賞賛
返信

5,869件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi victorien

you can look at latest L2.6.35_1.1.0 BSP patches:

L2.6.35_1.1.1_UPDATER_PATCH_UP :

The purpose of this patch release is Fix the updater.sb boot issue in the i.MX28 Linux BSP L2.6.35_1.1.0 release

I.MX28_MFG_TOOL_LINUX : Tool and documentation for downloading i.MX28 image during manufacturing.

Size (K): 33397 Format: gz Rev #: L2.6.35_1.1.0 Modified: 2/22/2013

L2.6.35_1.1.0_ER_SOURCE : i.MX28 Linux 2.6.35 Source Code Files and documentation.

Size (K): 726912 Format: gz Rev #: L2.6.35_1.1.0 Modified: 2/22/2013


Best regards

igor

0 件の賞賛
返信

5,869件の閲覧回数
victorien
Contributor IV

Thanks for your answer. and for giving more detail :

- I don't use ltib to generate the kernel

- I use mfg tool for windows (1.6.2.048)

- I generate my own updater_ivt.sb for my board (no problem with bootlet and zImage)

- I tried the modification from the patch but it change nothing

I find a test where mfgtool works fine :

- generate updater_ivt.sb for my own board

- execute mfgtool with this file

- I see the kernel boot on the board console

- the last line of the boot is : root@freescale /$ g_file_storage gadget: high speed config #1

- after that, ont the console I did : 'enter' uuc 'enter'

- then mfgtool communicate with my board

I think that it's my initramfs.cpio.gz which is bad and don't launch uuc. Do you confirm that ? Where can I find a boot initramfs.cpio.gz ? or how can I generate it ?

Best regards

0 件の賞賛
返信

5,869件の閲覧回数
victorien
Contributor IV

With the information that you give to me, I need LTIB. I'll try to install but but is there another way to generate this image ?

0 件の賞賛
返信

5,869件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi victorien

I am afraid that updater for MFG Tools can be generated only with ltib.

~igor

5,869件の閲覧回数
pt
Senior Contributor I

Hi

Generate image of type initramfs.

Screenshot from 2014-10-31 17_04_48.png

Screenshot from 2014-10-31 17_04_39.png

Regards

Pt

5,869件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

there were initramfs fixes in latest L2.6.35_1.1.0 BSP patches:

L2.6.35_1.1.1_UPDATER_PATCH_UP :

0 件の賞賛
返信