Issue in porting Kitkat to iMX6 Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Issue in porting Kitkat to iMX6 Board

跳至解决方案
2,077 次查看
sandy123
Contributor II

Hi Everyone,

When we tried to port Android Kitkat over our custom iMX6-Solo board, we faced several performance issues. For instance, we were not able to run game applications which show CPU usage above 90%. We didnt face these issues while porting Jellybean to our board though it uses the same kernel version as that of kitkat. Is our issues related with GPU?

标签 (4)
1 解答
1,741 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi san,

There is available a BSP of Android KitKat for i.MX6SL, you can find it here: IMX6SL_EVK_KK442_100_ANDROID_DEMO_BSP.

It is good to remember that the SoloLite doesn’t have 3D GPU, and the one included on the Solo (Vivante GC355) is not the same than the one on the Quad/Dual (Vivante GC2000).

So, it could be possible that some characteristics differ between platform and Android version, so, if you have specific GPU requirements, you could try checking the graphics libraries of each version.

Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,742 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi san,

There is available a BSP of Android KitKat for i.MX6SL, you can find it here: IMX6SL_EVK_KK442_100_ANDROID_DEMO_BSP.

It is good to remember that the SoloLite doesn’t have 3D GPU, and the one included on the Solo (Vivante GC355) is not the same than the one on the Quad/Dual (Vivante GC2000).

So, it could be possible that some characteristics differ between platform and Android version, so, if you have specific GPU requirements, you could try checking the graphics libraries of each version.

Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,741 次查看
sandy123
Contributor II

Thank you Carlos for the above information.

0 项奖励
回复