Issue about DDR settings on Boot Config

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue about DDR settings on Boot Config

903 次查看
tony_l_cai
Contributor III

Hi,all

     Our customize board is i.MX6DL,we use 4 pics of 16bit DDR3, so should we set the BOOT_CFG3[5:4]=10, which means

DDR Memory Map default config is "4KB Interleaving Enabled"?

     But I found, after we set DDR Memory Map default config as 00(Single DDR channel), it can work well. So could you give me more info about how to set this DDR boot config. 3Q!

标签 (2)
0 项奖励
回复
1 回复

778 次查看
igorpadykov
NXP Employee
NXP Employee

Hi tony

"4KB Interleaving " mode is applicable only for LPDDR2 2-channels mode:

one channel for even 4K, other for odd 4K addresses.


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------


0 项奖励
回复