Issue about DDR settings on Boot Config

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue about DDR settings on Boot Config

1,199件の閲覧回数
tony_l_cai
Contributor III

Hi,all

     Our customize board is i.MX6DL,we use 4 pics of 16bit DDR3, so should we set the BOOT_CFG3[5:4]=10, which means

DDR Memory Map default config is "4KB Interleaving Enabled"?

     But I found, after we set DDR Memory Map default config as 00(Single DDR channel), it can work well. So could you give me more info about how to set this DDR boot config. 3Q!

ラベル(2)
0 件の賞賛
返信
1 返信

1,074件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi tony

"4KB Interleaving " mode is applicable only for LPDDR2 2-channels mode:

one channel for even 4K, other for odd 4K addresses.


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------


0 件の賞賛
返信