Is there any problem with attaching csf data in address not aligned to 0x1000?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there any problem with attaching csf data in address not aligned to 0x1000?

跳至解决方案
1,258 次查看
krishnanp
Contributor III

I have question in Secure boot procedure.

Can I attach the csf data in an address which in not aligned to 0x1000 (4096).

I understand this alignment applicable to  run instance (after copied to RAM).

Please advice.

Krishnan

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
1,165 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Krishnan

there is no problem. CSF layout and alignment requirements

are described in HAB4_API.pdf document included in

IMX_CST_TOOL : Freescale Code Signing Tool for the High Assurance Boot library.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,166 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Krishnan

there is no problem. CSF layout and alignment requirements

are described in HAB4_API.pdf document included in

IMX_CST_TOOL : Freescale Code Signing Tool for the High Assurance Boot library.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复