Is there any problem with attaching csf data in address not aligned to 0x1000?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any problem with attaching csf data in address not aligned to 0x1000?

ソリューションへジャンプ
1,294件の閲覧回数
krishnanp
Contributor III

I have question in Secure boot procedure.

Can I attach the csf data in an address which in not aligned to 0x1000 (4096).

I understand this alignment applicable to  run instance (after copied to RAM).

Please advice.

Krishnan

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
1,201件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Krishnan

there is no problem. CSF layout and alignment requirements

are described in HAB4_API.pdf document included in

IMX_CST_TOOL : Freescale Code Signing Tool for the High Assurance Boot library.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,202件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Krishnan

there is no problem. CSF layout and alignment requirements

are described in HAB4_API.pdf document included in

IMX_CST_TOOL : Freescale Code Signing Tool for the High Assurance Boot library.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信