Is there any problem with attaching csf data in address not aligned to 0x1000?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any problem with attaching csf data in address not aligned to 0x1000?

Jump to solution
1,259 Views
krishnanp
Contributor III

I have question in Secure boot procedure.

Can I attach the csf data in an address which in not aligned to 0x1000 (4096).

I understand this alignment applicable to  run instance (after copied to RAM).

Please advice.

Krishnan

Labels (1)
Tags (4)
0 Kudos
Reply
1 Solution
1,166 Views
igorpadykov
NXP Employee
NXP Employee

Hi Krishnan

there is no problem. CSF layout and alignment requirements

are described in HAB4_API.pdf document included in

IMX_CST_TOOL : Freescale Code Signing Tool for the High Assurance Boot library.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,167 Views
igorpadykov
NXP Employee
NXP Employee

Hi Krishnan

there is no problem. CSF layout and alignment requirements

are described in HAB4_API.pdf document included in

IMX_CST_TOOL : Freescale Code Signing Tool for the High Assurance Boot library.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply