Is there a way to wake up IMX6Q via ethernet interrupt?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there a way to wake up IMX6Q via ethernet interrupt?

跳至解决方案
1,409 次查看
gkt
Contributor II

Hello all.

I am testing the sleep modes of IMX6QSABRESD. I can wake up the processor by using UART interrupt as it is mentioned in the Linux Reference Manual.

However, is there a way to wake up IMX6Q processor by using ethernet interrupt? 

Thank you in advance.

标签 (2)
0 项奖励
回复
1 解答
1,265 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Giray

please check patch on

Wake on lan in mx6 sabresd board 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,266 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Giray

please check patch on

Wake on lan in mx6 sabresd board 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------