Is there a way to wake up IMX6Q via ethernet interrupt?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a way to wake up IMX6Q via ethernet interrupt?

ソリューションへジャンプ
1,460件の閲覧回数
gkt
Contributor II

Hello all.

I am testing the sleep modes of IMX6QSABRESD. I can wake up the processor by using UART interrupt as it is mentioned in the Linux Reference Manual.

However, is there a way to wake up IMX6Q processor by using ethernet interrupt? 

Thank you in advance.

ラベル(2)
0 件の賞賛
返信
1 解決策
1,316件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Giray

please check patch on

Wake on lan in mx6 sabresd board 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,317件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Giray

please check patch on

Wake on lan in mx6 sabresd board 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------