Hi,
My HW, TX and RX are connected together, with a 1K resistor in the middle. Then connect to the UART debug board (the debug board can enumerate a UART port for communication, and has single-line and dual-line UART conversion function).
My assumption is that when use TX, disable RX, and when use RX, disable TX. But I don't know how to disable TX or RX.
MCU: RT595
Hello
Hope you are well.
Unfortunately, we don´t have an example using 1-wire UART.
I apologize for the inconvenience this may cause you.
To disable RX and TX you need to disable the corresponding FIFO in FIFOCFG register.
If you have more questions do not hesitate to ask me.
Best regards,
Omar