Is there a demo about 1-wire uart in the rt595 SDK?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is there a demo about 1-wire uart in the rt595 SDK?

1,040 次查看
Dave_SU
Contributor III

Hi,

My HW, TX and RX are connected together, with a 1K resistor in the middle. Then connect to the UART debug board (the debug board can enumerate a UART port for communication, and has single-line and dual-line UART conversion function).

My assumption is that when use TX,  disable RX, and when use RX, disable TX. But I don't know how to disable TX or RX.

MCU: RT595

标记 (1)
0 项奖励
回复
2 回复数

1,021 次查看
Dave_SU
Contributor III

@Omar_Anguiano 

thanks, let me try it.

0 项奖励
回复

1,033 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.
Unfortunately, we don´t have an example using 1-wire UART.
I apologize for the inconvenience this may cause you.
To disable RX and TX you need to disable the corresponding FIFO in FIFOCFG register.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 项奖励
回复