Is it possible to use a chip designed for single SPI line with QSPI lines on the i.MX8MPlus?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to use a chip designed for single SPI line with QSPI lines on the i.MX8MPlus?

ソリューションへジャンプ
863件の閲覧回数
puiyee_poon
Contributor I
0 件の賞賛
返信
1 解決策
839件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which boot flash have on your board?

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
840件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which boot flash have on your board?

0 件の賞賛
返信
804件の閲覧回数
puiyee_poon
Contributor I

We need SRAM in our design but we don't have any single SPI lines left from the processor due to the processor only supports 3 SPI interfaces and they are already occupied. Therefore we wonder if it's possible to connect a single SPI SRAM on the QSPI-port (where the pins are multiplexed with NAND-pins) from the processor. 

0 件の賞賛
返信