Is it possible to use a chip designed for single SPI line with QSPI lines on the i.MX8MPlus?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to use a chip designed for single SPI line with QSPI lines on the i.MX8MPlus?

Jump to solution
921 Views
puiyee_poon
Contributor I
 
0 Kudos
Reply
1 Solution
897 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which boot flash have on your board?

View solution in original post

0 Kudos
Reply
2 Replies
898 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which boot flash have on your board?

0 Kudos
Reply
862 Views
puiyee_poon
Contributor I

We need SRAM in our design but we don't have any single SPI lines left from the processor due to the processor only supports 3 SPI interfaces and they are already occupied. Therefore we wonder if it's possible to connect a single SPI SRAM on the QSPI-port (where the pins are multiplexed with NAND-pins) from the processor. 

0 Kudos
Reply